Tag Archives: Heavycon EVO

Plastic VS Aluminium – Heavycon Edition

From |

Heavy-duty connectors are typically made of aluminium as it is supposed to be tough and durable. However, being an innovative company and discontented with the current industrial norm, Phoenix Contact had come up with HEAVYCON EVO in plastic.

The plastic used in HEAVYCON EVO housing is not just any normal plastic, it is made of polyamide, reinforced with glass.

So, how strong is strong? Several tests were done to the plastic HEAVYCON including basic IP and NEMA tests in accordance with DIN EN 60529, NEMA 250. This ensures that the contact inserts within the plastic housing are protected against the ingress of dust and heavy jet water. The other tests include:

Vibration test in accordance to IEC 60068-2-6

Harmonic, sinusoidal vibration is applied to HEAVYCON plastic housing to simulate rotating, pulsating or oscillating forces. HEAVYCON plastic housing fulfils these requirements, making it ideal for heavy machinery application.

Temperature shock test in accordance to IEC 60512-11-4

We simulate significant temperature changes by switching HEAVYCON plastic housing between 2 chambers of extreme temperatures within seconds. The result is affirmative – HEAVYCON plastic housing is suitable to be used in applications with ambient temperature between -40 to 125 degree Celsius.

IK shock test in accordance to IEC 62262

Shock is introduced by dropping a hammer of 1.7 kg mass from a height of 0.3m. HEAVYCON plastic housing is able to meet the mechanical requirements similar to the HEAVYCON aluminium housing.

Roll over test in accordance to DIN IEC 62196-1

This is a special test carried out on the plastic housing where a forklift truck weighing several tons rolls over it. HEAVYCON plastic housing is able to withstand high amounts of stress from heavy, moving loads without any adverse effects on its function. In fact, in Singapore, we proved it again by driving a car over the connector.

Dynamic load test

Besides the strength of the plastic housing, we have to ensure the latching mechanism is heavy-duty enough as well. In this test, we applied a force of 200N to the cable at an angle of 90 degree. This is to test the HEAVYCON EVO bayonet as well as the locking latch between the housing and panel mounting to make sure that they do not malfunction under extreme static load.

Through the tests we have done, we can conclude that plastic can be as strong as metal too, in this case aluminium. To find out more about the durability of our HEAVYCON EVO in plastic, leave us an email at marketing@phoenixcontact.com.sg!

Heavycon Evo

From |

*Sigh*

I believe that many of us have experienced similar problems with plugs and sockets as pictured above, especially while travelling. Due to poor designs, some of our bulky charging equipment for our phones, laptops or cameras may not be able to charge. This creates massive inconvenience for us as we are unable to use our devices when we need them. In times like these, being able to adjust the wall plug orientation would solve the problem.

Surprisingly, such problems also arise in factories and warehouses that usually utilise heavy machinery. However, having such problems with heavy machinery will bring about more inconvenient repercussions such as having to move your machine to another location or adjusting your wall plug so that the socket can be plugged into it. These will bring about higher costs and also more tedious work.

The Phoenix Contact team has thus come up with a solution to overcome these problems.

Our Heavycon Evo is a heavy duty connector which allows the cable gland to be connected vertically or horizontally depending on the site conditions and requirements. The housing offers range from B6 to B24 and cable gland sizes of M20, M25, M32 and M40. Because of how customisable the product is, using it reduces the inventory in stock. Heavycon Evo is particularly useful when it comes to installation of cables in rather tight spaces. This also helps create a more compact setup which saves space. In cases where the wiring and connection points between cables are in obscure and inconvenient positions, the Heavycon Evo allows the user to alter the orientation of the sleeves from horizontal to vertical or vice versa. This feature also allows the wiring to last longer as the wires will not be in positions where they are under high tension.

Besides fulfilling its original purpose, the Heavycon Evo has additional benefits. When told that the Heavycon Evo is made up of plastic, many have the impression that it is not very durable. However, the fact that the Heavycon Evo is made of plastic brings about many benefits. The Heavycon Evo is made of high grade polyamide plastic that has gone through stringent quality checks such as IP and Nema degrees of protection, vibration, temperature shock, shock resistance, roll-over test and the dynamic load special test which verifies that the Heavycon Evo bayonet locking and double latch do not open independently or malfunction even in the case of extremely high static loads. Furthermore, the high grade plastic of Heavycon Evo will drastically lessen the load of machinery as it is significantly lighter than its metal counterpart by up to 50%.

Heavycon Evo enables the multiple connections of data, power and signal in a single housing with up to six difference combinations. We have also implemented our state of the art push-in technology in our inserts to allow easy, fast and secure connections in every application. Lastly, there is a common misunderstanding that plastic sleeves cannot match the applications of metal sleeves. However, this is not true as our Heavycon Evo is compatible with all existing setups of up to 24 positions with existing metal setups.

In conclusion, Heavycon Evo is compact to be installed in tight positions, cost effective, light weight and compatible. Hence, it will be your number one choice when buying heavy duty connectors.

Interested to find out more? Feel free to contact us at marketing@phoenixcontact.com.sg!

Heavy-duty connectors for every application

From |

Heavycon complete heavy-duty connectors from Phoenix Contact offer a reliable seal up to degree of protection IP69K. There are matching plug-in connections for every requirement with housings from three series types and matching contact inserts which can be combined.

4727

The standard series offers a wide range of robust metal housings with various different cable outlet directions and locking mechanisms. The flexible, swiveling bayonet locking of the EVO series allows the cable outlet direction to be freely selected and reduces the number of versions and thereby the warehousing costs by up to 70%. Not only does the direct screw locking without panel mounting base result in cost savings, it also means that the Advance housings are particularly durable and robust.

All components can be individually combined and flexibly modified, extended or exchanged. The standard and EVO housing is pin-compatible with the market standard and the Heavycon metal housing is “EMC-ready” thanks to conductive surfaces and seals. Combined with shielded cable glands, they offer you reliable protection in electromagnetic surroundings. All housing series fit standard panel cutouts.