Category Archives: Industrial Electronics

Safe and Reliable Power

From |

Upon mentioning PCB connection or PCB connectors, one of the first things that usually come to mind is an Electronics board for various applications. When electronics are involved, most manufacturers of connectors cater their designs to digital applications for modern devices such Smartphones, Tablets, Laptops, LED TVs, Set-Top Box and simple remote controllers.

For the above mentioned, design engineers, electronics designers, field application engineers, sales engineers and module designers often overlook the challenges or requirements needed for Industrial Electronics.

Most PCB or Industrial Control boards in Industrial Electronics are required to take-in high levels of in raw current, for the heavy duty tasks of operating motors, sensors and measuring equipment needed on modern devices.

New generation versions of Vision Inspection, Test System, Pick & Place, Bonding, Dicing, Conveyors and Ovens, utilizes loads that go up to 60A and 80A AC Voltage.

Typically, such high current capacity demands stringent safety features and equipment to be rigorously tested in high temperatures to ensure reliability and safety, in order to prevent catastrophic breakdowns of such systems.

From Phoenix Contact’s vast array of devices, Combicon Power is tried and tested to be the most suitable and reliable High Power Connector available in the market. Phoenix Contact’s Combicon Power are certified in UL, VDE and EAC, to ensure standards are in place giving customers ease of mind when adopting Combicon Power.

Combicon Power

Phoenix Contact’s MKDS 10, MKDSP 10HV, IPC 16, PC 16, PC 4, PC 5, HDFK and UW, were all adopted and used in two of the most notable Test and Management MNCs in Malaysia, in the Test and Measurement Systems produced by these MNC.

When your applications, products or modules are Power Hungry, and yet you need a safe, proven and reliable Power Connectors, Combicon Power is the answer to your needs and concerns.

Feel free to contact us to find out more!

Cable Entry System – CES

From |

Have you ever left your earphones in your pocket and when you wanted to use them again, they emerge as a tangled ball of mess? Annoying, isn’t it?

Well, the wiring of current and conventional electrical panels brings about a similar problem. The above picture shows its set up and at a glance, three words pop up in my mind: Complex; Costly; Time-consuming.

So why is this so?

Firstly, in the current system, multiple holes of different sizes need to be drilled in accordance with the cable sizes. Imagine the hassle having to drill ten holes of different diameter just to see messy wires intertwined together.

Next, a common occurrence to such wiring systems is the need to add additional cables. If you are lucky, there will be enough space on the flange plate to drill the extra holes. However, if the space is insufficient, or if you need larger holes for new cables, you would most likely have to replace the entire electrical panel and redo the entire wiring system from scratch. Not only does this add on to the hassle, it also adds on to labour and cost.

Lastly, conventional wiring systems require more time to rectify problems in communication. This is due to the difficulty in identifying specific cables especially when they are bundled together. The troubleshooting process thus leads to longer downtime which means financial losses for the company.

The Solution

Phoenix Contact has thus come up with a solution to eliminate this problem. Our Cable Entry System (CES) comes with specific features to tackle the hassle of the conventional system.

Firstly, only one or two holes would have to be cut to enable installation of up to ten cables in the system, greatly reducing the set up time. Furthermore, the CES can cater to different cable diameters ranging from 2mm-24mm. All these can be easily installed by mounting the sleeves of varying sizes on to the robust metal reinforced frame.

Next, additional cables can be installed by removing the blind sleeves from the extra cable holes provided by the CES. In the event that the existing cable configuration has to be amended, the CES allows for easy reassembly just by replacing the sleeves with those of different cable diameters. This eliminates the trouble of cutting out new holes on the flange plate.

Lastly, the CES allows cables to be easily identified as the rectangular frame organizes the sleeves holding the cables in an orderly manner that is easy on the eyes.

Besides tackling the inconveniences of the conventional electrical panel wiring, the CES offers protection class of IP54, making it suitable for harsh environment conditions.

If your current electrical wiring system reminds you of your ball of tangled earphones, it‘s about time you switch to Phoenix Contact’s Cable Entry System. Our CES will be the solution to increasing your productivity and cost saving to your electrical panels wiring.

Interested to find out more? Contact us at marketing@phoenixcontact.com.sg!

LV Compartment for MV Switchgear

From |

Box by box towards Smart Grid 1: LV Compartment for MV Switchgear

The gradual shift towards the much vaunted Smart Grid structure has been gathering steam in the last few years. While much of the excitement has been generated from the immense potential of what a fully completed Smart Grid system can bring (for example, higher reliability at reduced cost), Grid operators, independent power producers and their team of engineers are facing real difficulties in implementing such systems today. It is easy to talk about wanting to implement technologically advanced systems, but when it comes to actually executing the projects to implement such solutions, the complexity surrounding such implementations comes to the fore.

Much of this complexity arises because of the vast variety of applications within the industry. It is particularly difficult to find the right set of products that are suitable for the application, reliable, fast to set up and easy to manage. For example in Transmission and Distribution substations, there will minimally be systems for transformers, shunt reactors, switchboards, intrusion detection monitoring systems and each of these systems can consist of smaller sub systems. For example, in monitoring a switchboard, we can monitor downstream load current for energy balancing; micro current fluctuations for signs of partial discharge or even for predictive maintenance; door contact monitoring for physical security and the list goes on. Each of these systems will require the right set of products and will have to be linked in this web of madness. Imagine the chaos!

At Phoenix Contact, we recognise this difficulty. While we have many solutions for Energy Industry that we are always sharing with the various stakeholders, in this series of blog articles, we will be examining how we help to simplify the implementation of Smart Grid. We will do so by examining the building blocks of a system – the individual panels which form up a system; and we will do so box by box. This first article will be about LV Compartment of MV Switchgear and we will delve straight into the 3 problems switchgear builders and grid operators are facing!

Problem 1: How do I collect signals from my switchgears and transform it into IEC61850?

The completed substation topology will involve decentralised controls where IEDs are placed at high voltage equipment (on transformers and switchgears) itself. Even when it is not completed, communications from the bay control cabinets and protection devices to the substation control system are being converted to IEC61850 as IEC61850 has proved to be a superior communication protocol and standard to reduce downtime and increase reliability of the grid. Therefore, it is only a matter of time before all switchgears are converting signals from the circuit breakers and all other auxiliary signals into IEC61850 data. However, examining the LV compartment of switchgears today, the signals are still being passed out with many copper wires or connected to numerical relays. These present two clear drawbacks:

  1. There are a lot of copper wires going out of the panel or into numerical relays. The associated cost includes requiring marshalling or pilot cabinets and related components and regular maintenance to check if the connections are good. In addition, it is difficult to isolate where the fault is when there is a loss of signal. In the worst case scenario, there might even be accidental shorting resulting in severe downtime!
  2. Numerical relay and its I/O cards are expensive.

These result in higher initial cost and higher eventual maintenance cost with downtime not necessarily minimized, especially in the event of loss of signal.

Using of a Bus coupler capable of communicating via GOOSE and MMS will solve both of these problems. Using Phoenix Contact bus coupler as an example, the signals can be easily inserted and aggregated as IEC61850 data. It certainly reduces the number of cables leaving the cabinet and with the light indicators, you can see clearly which connections are good without requiring extra tests. It is also of lower cost compared to numerical relays’ IOs while communicating perfectly with them.

Problem 2: There are too many wires, how can we manage them better?

Being the founder of the original ceramic terminal block, it is already tempting to say that Phoenix Contact is the best at solving this! But in the last few years, we have developed more data connectors to put us in a better position to solve this for switchgear builders!

We have an extremely wide range of terminal blocks for every applications and needs. We have demonstrated to be able to meet each and every customers’ unique demands, be it requiring pluggable solutions, fastest connection technology, space saving, you name it, we’ve done it!

In this article, we would just like to highlight how a commonly used connector for switchgears has developed to adapt to Smart Grid. In the past, our Heavycon (heavy duty connector) was often sold to connect the LCC and Bay cabinets. This enabled quick connection on site.

However, these connectors are usually for loose copper wires only. Although you can strip an Ethernet/serial connector to use such connectors, these connectors does not cater very well for the shielding required for data connector. Therefore, Phoenix Contact has developed a modular connector, allowing you to use your data connectors directly! This modular connector even allows you to have connectors which allow for high power!

Problem 3: With more signals being collected, there will be more testing to be done. How can we ensure we are safely doing the testing all the time!

Every so often, testing needs to be done on the current transformers and voltage transformers regularly. For current transformer especially, if not done right, explosions can happen. Currently, the shorting and breaking of circuits are done manually by hand (yes you read that right) and as you can imagine, explosions lead to death.

To solve this, Phoenix Contact has developed our test disconnect system (FAME) where shorting is done automatically and it is fool-proof!

Instead of using terminal blocks that are switched manually, you can replace it entirely with FAME and from then on, every testing procedure will be done how it is meant to be done: SAFELY.

We have assembled this product into a demo box along with other products that Phoenix Contact offers for LV Compartment for MV Switchgear. If you will like to have a look at the demo box up close, do contact us at marketing@phoenixcontact.com.sg and we will get in touch!

FL 2000 Managed Switch for Railway Applications

From |

Highspeed commuter trainFor many years, Phoenix Contact has been a reliable partner of the Railway Industry, supplying products such as Power Supply Unit, Terminal Blocks, Heavy Duty Connectors for railway applications. In the recent years, Phoenix Contact has invested a significant amount of effort to create innovative products such as controllers and ethernet switches for automation applications.

Ethernet-based communication medium/protocols are becoming the norm in modern automation environments. Traditional serial-based communication medium/protocols are unable to support the requirements for transmission speed and data size; especially for time-critical applications.

FL 2000 Managed Switch

Phoenix Contact's FL 2000 Managed SwitchThe new FL 2000 Managed Switch was officially launched in April 2017 during the Hannover Fair. This new series of Ethernet Switch was specifically developed to bridge the gap between simple unmanaged switches and complex managed switches which are already available within Phoenix Contact product portfolio.

In railway applications, data integrity is especially critical to ensure the smooth and safe operations of the system. Transmission distances from various subway station control systems to the main control center are often in the range of kilometers, which conventional copper-based medium cannot handle. The only way to transmit the data over long distance is via Fiber Optic technology.

Our sales team spotted an opportunity to propose our FL 2000 Switch in one of the railway system upgrading project in this region. We managed to overcome several challenges despite facing strong competitions from various industrial giants. The main unique selling points of our FL 2000 Switch that met with approval of the end user and system integrators were:

  • Feature important automation features with attractive price/performance ratio
  • Easy/Flexible Configuration/Setup
  • Comprehensive approvals to meet stringent industry-specific approval requirements
  • Various connection port options: Copper and Fiber Optics; Gigabit network possible

In addition, we are also able provide a bundle offer including our UPS and Power Supply Unit.

If you would like to find out more about our FL2000 switches, check out our website or you can leave us your contact and we will get in touch with you as soon as we can.

Phoenix Contact – Your Partner in Safety and Reliability for Railway Industry

From |

RailwayPhoenix Contact has been serving the railway industry for decades, especially for rolling stock and signalling. Safety and reliability has always been our number one concern when developing products for railway applications.

Safety on Board

The basic requirement for safety and reliability is standard compliance. Phoenix Contact has been certified by the International Railway Industry Standard (IRIS) since April 2008 and this standard is based on the quality management standard DIN EN ISO 9001, which has been extended with international railway-specific requirements. The ongoing tests during the development and production cycle of the products are essential to guarantee the product quality.

On top of that, all rail-specific products from Phoenix Contact fulfill the standards of DIN EN 50155, an international standard covering rolling stock; DIN EN 50121 electromagnetic compatibility; and EN 45545, fire protection on rail vehicle. Besides, shock and vibration test, material test and other fire protection is also critical for the railway application.

Safety should not be limited to the big ticket items and should even be extended to the passive component level. For example, the cable markings like shrink sleeve should be halogen-free and fulfill DIN 5510-2 with an oxygen index of 34.9%. besides being halogen-free, the cable ducts should enable individual bars to be broken without using any tools or resulting in any burr through defined breaking points according to EN 45545-2 (R22/R23:HL3). Behaviour in fire is another key concern and the plastic used for Phoenix Contact’s terminal blocks is halogen-free polyamide PA 6.6; which meets the highest safety requirement of UL 94 V0.

Push-in Terminal Blocks and Marking

Push-in Terminal Blocks and Marking

Cable Management

Cable Management

Network on Board

Nowadays, commuters demand for “Internet on board” has made the information and infotainment systems essential in trains. The M12 network connectors with a mechanically robust design, in compliance with IEC 61076-2-101, together with high quality cables meeting the requirement of EN 45545-2 will ensure reliable communications. The heavy-duty connector, compliant with IEC 61373, with modular contact inserts form a flexible and safe transmission of signal and power circuit on rolling stock carriage connection and simultaneously ensures comprehensive protection in the event of electromagnetic interference fields.

Halogen-free Polyamide PA 6.6

Halogen-free Polyamide PA 6.6

M12 Network Connector

M12 Network Connector

Surge Protection

Surge voltages and lightning strikes are common issues in signalling, hence the surge protective device (SPD) become significantly important to maintain reliable signal transmission. Phoenix Contact’s SPD has been tested according to IEC 61643-21 and the plug can be disconnected for test and maintenance by using the portable test laboratory. According to IEC 62305-3, the SPD must be tested regularly and the test values should be documented and traceable. Additional features like multi-stage monitoring (green – operating, red – fail and yellow – reach performance limit) for predictive maintenance and remote signalling for early detection of overloaded SPD can help to further enhance reliability.

HEAVYCON HPR

HEAVYCON HPR

HEAVYCON Modular Inserts

HEAVYCON Modular Inserts

Signal SPD with multi-stage monitoring (PT-IQ)

Signal SPD with multi-stage monitoring (PT-IQ)

Signal SPD with remote signalling (TTC)

Signal SPD with remote signalling (TTC)

Power Supply

The power supply unit (PSU) is used to convert main AC to low-voltage regulated DC power and it should at least be compliant with EMC Directive 2014/30/EU, IEC 60950-1, DIN EN 61558-2-16 and UL 508. To ensure smooth operation and maximum uptime, the redundancy setup of the power supply cannot be overlooked.

A redundant system can made up of two power supplies and a diode or Phoenix Contact’s O-RING to prevent back flow of current. An ORING being a more advanced and modern redundancy module compared to the diode, comes with auto-current balancing (ACB) technology which ensures the power supplies work equally hard. This enables the power supplies to have a longer and more consistent lifespan.

The redundancy status as well as the status of the ORING can be monitored, whereas this cannot be done with a DIODE. The PSU becomes more reliable and dependable when it is capable of sending analogue signals to control system on measurement values such as real time current, voltage and power for early detection of operational fault as well as critical information to the user.

QUINT 4 Power Supply With Diode

QUINT 4 Power Supply With Diode

QUINT ORING with ACB

QUINT ORING with ACB

Transporting You into the Future

Phoenix Contact will continue to develop the products or solutions that suit railway application and safety and reliability will always be the top concern on top of ease of installation, operation and maintenance.

To find out more about the solutions that Phoenix Contact has for the railway industry, check out our website or leave us your contact at marketing@phoenixcontact.com.sg and I will get in touch with you as soon as I can.

Quint Power – 4G Power Supply with NFC

From |

QUINT Power - 4G Power supplyHave you heard of Phoenix Contact’s QUINT POWER range of power supplies?

If you have not, where were you!

Our QUINT power supplies have been consistently making waves as THE power supply fit for any industrial use.

It is that good that Phoenix Contact has released the fourth generation of the high-performance QUINT POWER range, only this time it’s spearheading the industry by embracing the spirit of IIOT.

Tell us MORE about this QUINT

Our QUINT POWER is the one and only power supply in the market to incorporate Near Field Communication (NFC) technology.

This feature is the latest addition to the already proven power supply unit that comes with SFB (Selective Fuse Breaking) technology, preventive function monitoring, high noise immunity as well as Power Boost.

Wait, What’s Power Boost?

QUINT 4 Power Supplies dynamic boost

The Power Boost technology allows the power supply unit to withstand indefinitely 125% or tolerate up to 200% of its maximum rated output current for 5 seconds without malfunctioning.

You heard that right, up to 200% of its maximum output current unlike others who would be fried to a crisp right about now.

Not just a Power Boost but empowering People too!

This technology allows users; engineers or technicians, to read and download configuration data of the power supply with any NFC enabled devices such as smartphones or tablets.

All you need is an Android device and you’re good to go.

This will also be handy at industrial sites during commissioning or maintenance where more often than not, there will be unforeseen circumstances where configuration cables are misplaced or worse laptops are not downloaded with the configuration software.

Another practical advantage is that the NFC technology allows configuration to be done in places that have low accessibility.

Examples are hard to reach places such power supply units that are installed at tight, very high or very low positions where it is difficult to carry a laptop.

Laptops can be bulky and requires a power supply to read power supplies (oh the irony). With smartphones and NFC, you could read data through the palms of your hands.

The QUINT POWER configuration App can be downloaded for free from the Google Play Store.

Say goodbye to legacy multi-meters and expensive devices!  Who says you can’t use your phones on the job.

I’m super excited now! Tell me more…..

Configuration data such as device details, output voltage, output characteristics, signalling and control input mode can now be read, configured and then be downloaded without any need for physical cabling to the power supply.

Surely with the QUINT you’ll be seeing increase in productivity.

Without the access baggage -laptop and configuration cable – it reduces the time needed for configuration especially for projects with large quantities of power supply units.

The QUINT POWER power supply range can be used in various industries such as oil and gas, transportation, water, marine, power and chemical facilities as well as in the factory automation and manufacturing facilities where reliability and technical superiority are highly valued.

So if you’re looking for POWER SUPPLIES, look no further.

Our QUINT 4 is your answer.

With NFC enabled you’ll be giving your business the power of electricity, in your hands.

https://www.youtube.com/watch?v=8tm-F6ylMos

If you are interested to find out more about our Power Supplies, check out our website or leave us your contact at marketing@phoenixcontact.com.sg and I will get in touch with you as soon as I can.

UPS IQ – Smart Power for Intelligent Transport System

From |

The Land Transport Authority (LTA) recently awarded a tender for the Intelligent Transport System (ITS) to one of their system integrator to setup effective system for monitoring of traffic situation at junctions. The system, which is part of the Smart Nation Initiative Program, will automatically alert the operator of the traffic volume so that remedial actions can be taken promptly.

Traffic Camera

Intelligent Transport System (ITS)

The Intelligent Transport System (ITS) is at the heart of what keeps us safe on the roads and tunnels system in our city. In land-scarce Singapore, ITS’s sophisticated traffic and control system will maximize road network efficiency capacity as well as monitor and manage the traffic flow.

The ITS infrastructure spans over 164km of expressways and road tunnel system, including Kallang-Paya Lebar Expressway(KPE), Marina Coastal Expressway (MCE), Central Expressway (CTE), Fort Canning Tunnel (FCT) and Woodsville Tunnel (WVT).

Our partner in Singapore has worked wholeheartedly with this system integrator, from design to testing and finally, to the implementation with our UPS-IQ.

Solution

Together with our partner, we set up the actual UPS and communication system to show to the system integrator. This was to provide the proof of concept to simulate the system. A demonstration of the UPSconfigure software allowed the UPS system to be integrated seamlessly into the innovative application from the special system by the system integrator. The system will be manned by LTA.

UPS IQ

UPS IQ

Key Features

  1.  High MTBF – Higher MTBF (>600,000 hours) as compared to most of our usual competitors ensures more reliabilty.
  2. Modbus Enabled – This has enabled the system to be communicated within the same network. It allows the system to be monitored from the main control room without additional hardware which translates into lesser points of failure and eventually to cost savings.
  3. Monitoring software (UPS Config) – The UPSconfigure feature allows the innovative application of the system integrator proprietary software to be integrated seamlessly into their application. This speeds up the deployment process and allows the system integrator to make more efficient time, labour and tools deployment.

If you would like to find out more about our UPS-IQ, check out our website or just leave us your contact at marketing@phoenixcontact.com.sg and I will get in touch with you.

Hybrid Motor Starters – CONTACTRON

From |

Phoenix Contact’s Contactron is a range of hybrid motor starters that is engineered and design to replace the traditional way of starting, stopping and managing the motor. And with that, it comes with numerous advantages and benefits to the system integrator, contractor and end user.

https://www.youtube.com/watch?v=Ap0iBA-BiqQ&t=63s

The most obvious advantage is the space savings it brings if one chooses to use Contactron instead of the using the usual contactors and thermal overload relay. The space savings can range from 50% to 89% depending on the motor configuration.

With space savings, one can design their panel or cabinet to be smaller. This is useful for sites where space is limited such as on top of a shipping port cranes. An even more remarkable savings can be achieved by using the Contactron to shrink the size of an Ex d explosion proof box by replacing the contactors and thermal overload relay.

Contactron comparison with traditional motor starter

Contactron setup compared to traditional motor starter setup

Secondly, the Contactron can very much reduce the downtime of a plant or factory as it can perform on average 10 times the typical service life of the traditional contactors. This is because, rather than depending on the ‘prone to failure’ nature of mechanical parts of the contactors, the Contactron uses a combination of solid state and electromechanical relay. Therefore, for motors that are subjected to frequent start stops, the Contactron is an obvious winner.

Besides that, the Contactron can be connected and communicated to a higher level control and monitoring system. This allows crucial information on statuses of the Contactron to be sent to the control system using common protocols such as Modbus, Profibus and Internet IP. This is crucial for visibility and productivity of the plant or factory operators. The traditional contactors with no intelligence have no possibility of being connected to a control system.

Besides, the above, there are many more advantages of using Phoenix Contact’s Contactron over traditional motor starters.

You can click here find out more about our Contactron Hybird motor starters

However, it will be best to be able to feel and learn about this with a face-to-face direct demonstration and presentation. If there is any interest, please feel free to leave us your contact at marketing@phoenixcontact.com.sg and we will arrange a visit to your office.

Let there be Light

From |

Let there be light: Phoenix Contact Components for Reliable Power Grids

On 7 July 2017, Phoenix Contact Singapore Team organised a’ Dining in the Dark’ event as part of Corporate Social Responsibility.  In the short 2 hours without our sight, we experienced a range of emotions such as fear and helplessness. This event also allowed us to understand the challenges that persons with visual impairment faced daily. It is truly a meaningful event that we are thankful to be able to experience with the friends we made from work.

Phoenix Contact's 'Dining in the Dark' CSR Event

Phoenix Contact’s ‘Dining in the Dark’ CSR Event

In today’s world, it might not be an exaggeration to say that we will feel the fear and helplessness if we do not have access to electricity. For a start, life-sustaining equipment in hospitals will not be in operation. Many of life’s conveniences such as lights, entertainment, air-conditioning etc. will be stripped from us. For this, electrical grids are always considered critical infrastructure all around the world and efforts are made to ensure the grid is always operating. Phoenix Contact contributes to this reliability with our products. Below are some examples:

    1. Terminal blocks (Clipline Complete)Clipline terminal blocks
      Our terminal blocks are widely used in power industry. For quick installation in Marshalling/Pilot panel, our customers prefer the use of

      • Push-in connectionThis connection method is fast, do not require special tools, safe, ensure consistent and good connection for every insertion and ideal for areas with high vibration. Most importantly, unlike screw connection, over time, push-in connection does not loosen.
      • QTC connectionThere is no need to strip the wire using QTC connection, making it the fastest way for wire installations. Moreover, Phoenix Contact QTC terminal blocks do not require special tools!
    2. Protection terminal blocksURTK-6 Test Disconnect Terminal Block

      Especially for CT testing, where you have to make the testing circuit before breaking the transformer circuit, it is important to ensure that the “make-before-break” is done properly! Failure to do so results not just in power outage, but often death.

      Our solution is our range of test disconnect terminal blocks, clearly labelled to ensure operators know exactly what is being done. There are also ample spaces for accessories for you to do the necessary bridging and testing.

      Offering inspiring innovations, Phoenix Contact has come out with a test disconnect system. Instead of manually doing the switching, why not let our system take care of it for you with Fast And Modular Energy system (FAME).

    1. DC/DC Converter and Power SupplyQUINT DC/DC converter and Power Supplies

      Usually in substations, there will be 110VDC power supply. However, most electronics components (remote IO, network switch, RTU) requires 24VDC/48VDC power input.  For this purpose, many substations around the world choose Phoenix Contact Quint IV Power Supply.

      Your advantages

      • SFB Technology selectively trips standard circuit breakers, loads connected in parallel continue working
      • Preventive function monitoring indicates critical operating states before errors occur
      • signalling thresholds and characteristic curves that can be adjusted via NFC maximize system availability
      • Easy system extension thanks to static boost; starting of difficult loads thanks to dynamic boost
      • High noise immunity, thanks  to integrated gas-filled surge arrester and more than 20 ms mains failure buffer time. Moreover, Phoenix Contact Quint IV Power Supply comes IEC61850-3 certified. This means that the unit can be used even for IEC61850 applications!
    1. Interposing relays
      With a wide range of relays, Phoenix Contact has the right solution for all standard relay applications, such as interposing relays.

      Your advantages

      • Easy handling, thanks to modern wiring and potential distribution concept
      • Easy extension to a timer relay, thanks to plug-in special function module
      • Complete product range covering all standard relay applications
      • Reliable system for high machine and system availability
      • Available as a complete module or modular system
Easy Wire Termination  Easy Power Distribution  Complete Product Range

Test Disconnect Push-in Connection

Our relays with push-in termination technology provide fast and easy tool-free wiring. Simply push the wire into the terminal , using very little force. Remove the wire by pushing done on the release button, using a screwdriver or ballpoint pen.

Test Diconnect Terminal Block Jumper

Reduce your wiring time up to 70 percent by using our modular terminal block plug-in bridges. These time-saving bridges ensure a reliable connection and reduces the possibility of wiring errors.

RIFLINE Complete

Switch currents up to 16 A. From coupling relays to a replacement for small power contactors; the product range offers the right relay for every application. Benefit from a uniform and consistent system

  1. Heavycon (Heavy-Duty Connector)
    Substations have high EMC and electrostatic interferences. They are also generally not places that people like to hang around in! Heavycon can help to reduce installation/maintenance time and at the same time, ensure reliable power/data/signal transmission. With a modular system, you can combine Fibre, Ethernet, Serial, signals, power all in 1 connector!

HEAVYCON Modular Connector

For example,

  1. the Local control cabinet can be connected quickly to the bay cabinet
  2. The Circuit breaker compartment can be easily disconnected/connected to the switchgear

Remote Monitoring via the Mobile Network

From |

Mobile Network Architecture

We are all available 24 hours a day. We have at least one cell phone, use the Internet on the go every day, and learn about the latest global news through our communication media. Having information at one’s fingertips is now essential to us all and nobody wants to give it up.

Think about the global competition in industrial production, which calls for us to continuously optimize our systems. As a production manager, you need to know at all times what is being produced worldwide on each machine, at what quality level and when the next maintenance interval is due. Such new systems are hardly imaginable today without efficient communication networks, which are essential for reliable system operation. This rapid development in the exchange of information and data that we have experienced in the telecommunications industry in the last few years is about to break into the industrial sector.

Indeed, many of these M2M (machine to machine) applications will be implemented over telecommunications networks. Now is the perfect time to consider these topics, applications, and technologies in the industrial sector.

Therefore I would like to share with you one of our success story implementing remote monitoring over the mobile phone network. The idea is to monitor remotely several paramaters on the oil well that is scattered in locations remotely using the GSM modem.

By doing this customer can get data more effective and efficiently compare to previously that one must go to every site locations and get information on the pressure and temperature at the oil well.

Solar-powered RTU

In this project we even integrate a solar system to power up the RTU and GSM modem since the location is remote and there is no power available. System architecture can be seen in the picture below:

RTU and Solar Power

Our GSM modem has a feature with dual sim cards which means when it detects low signal reception from one provider it can automatically transfer the communication to the other sim card. This is to maintain data availability.

We also set up a VPN tunneling in order to get a secure data transmission.

With this configuration, now customer is able to monitor oil wells data from office directly. They just need to select which location they want to monitor.

If you would like to know more on the remote communication using GSM modem, please do not hesitate to contact us. Thank you.