Are you looking for a basic monitoring relay that is ideal for simple monitoring tasks such as currents, voltages, 1- and 3 phases and phase sequence suitable for use in the building installation and in the production of machines and plants?
Category Archives: Industrial Electronics
RIFLINE complete
From |Would you like to have relays that enable quick and tool free cable wiring time?
Would you like to have relays that have the features of the terminal blocks such as marking materials, bridges and test adapters?
Would you like to have an option to transform a basic relay into a timer relay with three different functions?
New Highly Compact Isolation Amplifiers with Modular Group Error Logging
From |Five new products expand the function range of the highly compact Mini Analog isolation amplifier line from Phoenix Contact. The new fault monitoring system function also offers modular error logging in multi-channel applications.
Network Isolator Provides Reliable Protection in the Network
From |Phoenix Contact’s new FL Isolator 100-M12 network isolator provides reliable protection when electric potential differences occur. This galvanic separator is intended for heavy-duty use in all industrial Ethernet applications using M12 connection technology.
WLAN Ethernet Adapter for the 5 GHz Frequency Band
From |Phoenix Contact now offers an industrial WLAN Ethernet adapter for integrating Ethernet-capable devices into WLAN IEEE 802.11a/n networks (5 GHz frequency band).
Intelligent UPS Now Also Communicates with Higher-Level Controllers
From |IQ technology turns Phoenix Contact’s Quint UPS-IQ power supply into an intelligent UPS for the mounting rail that provides continuous information about the charging state, remaining runtime, and lifespan of its energy storage devices, thus maximizing system availability.
The new data cable now allows the UPS module to be integrated directly into the automation application.
New Bus Coupler for Fast I/O Systems
From |The Axioline real-time I/O system from Phoenix Contact has been supplemented by a Sercos-3 bus coupler. Its advantages include short reaction times and synchronized operation.
The New Generation of Motherboards for Signal Conditioning
From |The new generation motherboards Phoenix Contact Termination Carrier bridges the gap in the Phoenix Contact product range when it comes to connecting high quantities of signals to the process control level.
These Termination Carrier solutions connect system cabling via “Plug & Play” are state-of-the-art and are still in high demand, especially for system integrators.
High-Speed Profibus Extender for Railway Applications
From |Economic railway operation involves the cost-optimized management of buildings, reliable information systems, safe control of signals and data, as well as the constant and rugged use of components and systems in rail vehicles.
Fast WLAN for the Control Cabinet
From |With its industrial WLAN Access Point/Client WLAN 5100, Phoenix Contact presents a new device for wireless communication in accordance with the WLAN standard IEEE 802.11n.The wireless component supports the Mimo (Multiple Input Multiple Output) technology with three antennas.