Author Archives: alexanandharaj

Photovoltaic Monitoring System With Visualisation – A Project with ITE College East

From |

Photovoltaic (PV) Monitoring System With Visualisation

The Photovoltaic (PV) monitoring system was designed to monitor the performance of the PV panels’ output versus the temperature on the PV panel. There were two different types of PV panels used for monitoring, namely the mono-crystalline and amorphous silicone (Thin Film). The data that was collected were the DC output and the temperature on the PV panels.

Continue reading →