Chestnut Avenue Waterworks is one of the largest immersed membrane plant producing drinking water designed by Black & Veatch in Singapore .
The installation was one of a kind as permeate pumps was completely eliminated, commonly membrane train are used to draw water through the membranes and was replaced this with a siphon system taking advantage of the lie of the land. This solution eliminated 24 large permeate pumps and associated variable frequency drives and reduced capital and operating cost, reduced plant footprint and resulted in a very simple system to maintain.
And of course we are proud to announce that PUB Chestnut Avenue Waterworks is well protected from Surge & Lightning with Phoenix Contact Surge Protection Devices known as the PLUGTRAB.
httpv://www.youtube.com/watch?v=TNMMKGyZ898

Pingback: Tweets that mention See Phoenix Contact surge arrestor protecting a PUB water works installation. -- Topsy.com
Thanks for an idea, you sparked at thought from a angle I hadn’t given thoguht to yet. Now lets see if I can do something with it.
Couldnt agree more with that, very attractive article
nice post. thanks.
Terrific work! This is the type of information that should be shared around the web. Shame on the search engines for not positioning this post higher!