Some call it marking, others call it printing. At the end of the day, we require objects in our lives to be labelled, just like how every of us have a name or identification number. Before I joined Phoenix Contact 2 years ago, never did I know that Phoenix Contact offers such a wide range of marking possibilities!
At Phoenix Contact, we have 3 different technologies involved in our marking systems:
- Thermal Transfer
- LED-UV
- Laser
Thermal Transfer Printers
Our range of Thermal Transfer printers include Thermomark Roll, Thermomark Card, Thermomark Prime, and Thermofox.

Phoenix Contact’s Thermomark Roll, Thermomark Card, Thermomark Prime, and Thermofox utilise thermal transfer technology
This printing technology allows affording cost of printing, but yet allows text, graphics, batch numbers, and bar codes to be printed. Being economical and flexible, our Thermal Transfer printers allow users to do either batch printings, as well as continuous printings without wastage of materials!
LED-UV Printers

BLUEMARK CLED UV Printer
LED-UV: A revolutionary technology which is used in our Bluemark CLED printers. Not only does this marking system prints on plastic, it prints to aluminium too! The UV light will cure the ink and bond it to the material to ensure high resistance levels in various environments. The current markers allow marking of conductors, cables, and systems, covering the entire field of device and system marking!
Laser Printers

TOPMARK Laser Printer
Laser: Another groundbreaking marking system which uses a top class ytterbium fibre laser to mark on more than 400 different markers, ranging from stainless steel to aluminium to plastic. No ink or toner will be required due to the fact that the laser marks directly onto the marker material. Therefore, the resistance level of the markings are able to withstand the harshest environments and conditions, as long as the base material lasts!
CLIP PROJECT Software

CLIPPROECT Software
Just a single, free, software is required to design and send print jobs to Phoenix Contact’s range of printers. CLIP PROJECT has more functions that you can imagine, it even allows data to be automatically imported from Databases straight to prints. CLIP PROJECT and Eplan have been partners for quite some time, and this means that users can seamlessly allow direct printing in CLIP PROJECT straight from Eplan schematic. The CLIP PROJECT planning and marking software is all you need, and you may find more information of this software here.
Yes, it is free to download and free to use: No need to worry about having dongles for every computer, or annually paid subscriptions!