Tag Archives: interface

Power supply for industrial networks

From |

Incorporate Quint DC UPS easily and flexibly into existing networks

DC UPS with IQ Technology for industrial networksContinuing to supply machinery and equipment with power, even in the event of a mains failure, is imperative. Similarly, the ability of the UPS to communicate plays an important role in meeting this requirement. For that reason, we came with the new Quint DC UPS is the first intelligent and network-capable uninterruptible power supply for connecting to the Industrial Ethernet.

First of all, power fluctuations and the failure of the supply voltage generally result in an interruption in operations. In the worst-case scenario, it can result in a total plant failure. Many industry sectors use uninterruptible power supplies, or UPSs for short to avoid this and prevent downtime. This type of solution include three functional units: the power supply, the UPS itself, and the energy storage device. The power supply supplies energy to the load as long as the primary-side mains voltage is present. If the mains fail, the UPS takes over. It switches to the energy storage device so that the connected loads charge with power without interruption. After all, the required power becomes available by the energy storage device. Continue reading →

SOLARCHECK RSD Poll: Participcate to win a reflex camera

From |

SOLARCHECK RSD – Photovoltaic Panel Shutdown

SOLARCHECK RSD from Phoenix Contact makes working on photovoltaic systems so safe.

Solarcheck rsd

SOLARCHECK RSD consists of units for shutting down the individual photovoltaic panels and startup units, which are used to restart the system. Each shutdown unit disconnects the corresponding panel from the string group. The disconnection takes place automatically in the event of a fault and each time the inverter is shut down. The maximum value for the entire DC side of the photovoltaic system is then in the range of the safety extra-low voltage. There is no risk of an electric shock.

More on Photovoltaic panel shutdown

Show us that you are familiar with our PV Panels by participating in this poll. Select the right image, ‪VOTE and get a chance to ‪WIN an ‪SLR ‪‎camera!