Tag Archives: Traffic Monitoring

UPS IQ – Smart Power for Intelligent Transport System

From |

The Land Transport Authority (LTA) recently awarded a tender for the Intelligent Transport System (ITS) to one of their system integrator to setup effective system for monitoring of traffic situation at junctions. The system, which is part of the Smart Nation Initiative Program, will automatically alert the operator of the traffic volume so that remedial actions can be taken promptly.

Traffic Camera

Intelligent Transport System (ITS)

The Intelligent Transport System (ITS) is at the heart of what keeps us safe on the roads and tunnels system in our city. In land-scarce Singapore, ITS’s sophisticated traffic and control system will maximize road network efficiency capacity as well as monitor and manage the traffic flow.

The ITS infrastructure spans over 164km of expressways and road tunnel system, including Kallang-Paya Lebar Expressway(KPE), Marina Coastal Expressway (MCE), Central Expressway (CTE), Fort Canning Tunnel (FCT) and Woodsville Tunnel (WVT).

Our partner in Singapore has worked wholeheartedly with this system integrator, from design to testing and finally, to the implementation with our UPS-IQ.

Solution

Together with our partner, we set up the actual UPS and communication system to show to the system integrator. This was to provide the proof of concept to simulate the system. A demonstration of the UPSconfigure software allowed the UPS system to be integrated seamlessly into the innovative application from the special system by the system integrator. The system will be manned by LTA.

UPS IQ

UPS IQ

Key Features

  1.  High MTBF – Higher MTBF (>600,000 hours) as compared to most of our usual competitors ensures more reliabilty.
  2. Modbus Enabled – This has enabled the system to be communicated within the same network. It allows the system to be monitored from the main control room without additional hardware which translates into lesser points of failure and eventually to cost savings.
  3. Monitoring software (UPS Config) – The UPSconfigure feature allows the innovative application of the system integrator proprietary software to be integrated seamlessly into their application. This speeds up the deployment process and allows the system integrator to make more efficient time, labour and tools deployment.

If you would like to find out more about our UPS-IQ, check out our website or just leave us your contact at marketing@phoenixcontact.com.sg and I will get in touch with you.