Summary
- Aeon, the biggest shopping center in Johor, Malaysia, needed a solution to centralize their Existing Car Park Area, Extended New Car Park Zone & Shopping Mall Corridors Lighting Monitoring & Control system. Previously, their lighting controls were operated manually by switching the lights via a “ON/OFF” switch.
- The client was also searching for an alternative to reduce operational cost without compromising on safety and reliability.
- Phoenix Contact’s Malaysia team met their needs by producing a complete solution that reduced cost without substituting on safety and reliability.
- By utilizing Phoenix Contact’s solution, the client could now control their lighting centrally using pre-programmed scheduler to automatically switch the lights on or off without the need of additional manpower and monitor the system for lighting breakdowns or power outages.
- The client also achieved a decrease in energy consumption, essentially lowering the cost of operations.
- Overall, besides reducing their electricity intake and operational time, our solution allowed them to save cost in complex installations, hardware purchases, and future maintenance.
Customer Profile
The client, AEON, is the largest retailer in Asia with a retail network comprising around 300 consolidated subsidiaries and 26 equity-method affiliated companies ranging from convenience stores, supermarkets, and shopping malls.
One of their subsidiaries is located in Johor Bahru, Malaysia.
Officially opened in 2006, the shopping center is the biggest mall in Johor to date. It boasts the biggest hypermart and is located at Johor’s affluent area, making it the most visited mall especially on weekends.
Being a premium shopping center in Johor, they needed to explore options towards electrical efficiency and ensure this undertaking do not dampen the experience of their visitors.
Challenge: Improve energy and system efficiency without disrupting shopper’s experience
The client needed a Lighting Monitoring & Control System to reduce the operational expenditure of running a shopping mall. Since they operate from 10 am to 10 pm (which means that they’ll be switching the lights on at 8 am and will close later than 10 pm), they will have electricity running almost more than 12 hours a day.
Read more on how we’ve helped AEON Malaysia save more while doing less