Tag Archives: pc worx

OPC_UA SERVER for PC WORX-based Controllers

From |

Dynamic market changes make it necessary to solve automation tasks in line with Industry 4.0. The objective is always to produce more efficiently and intelligently. Uniform protocols, rules, and standards for communication are required to intelligently link machines and system components.

In the past, it was a very challenging task for any engineer to setup, access or share OPC classic remotely in a network but that has changed now, with Phoenix Contact’s OPC_UA Server.

The PC WORX UA SERVER from Phoenix Contact enables you to access all variables of PC WORX programmable controllers via the OPC_UA (Unified Architecture) standardized communication protocol.

Fig 1: System architecture with OPC_UA

Fig 1: System architecture with OPC_UA

Why you should switch to OPC_UA

The OPC Unified Architecture Standard, OPC_UA, is being adopted more widely across the market as the new market standard and provides the basis for open and standardized communication in the digital future.

OPC_UA Server capability:

  • Handle up to 200 controllers in a visualization or production control system
  • Variables are mapped via the standardized PLCopen profile
  • The OPC_UA server uses the binary protocol for communication, resulting in high data transmission speeds
  • A security concept based on certificates protects against unauthorized access
  • Status & Quality of connection for each individual items
Fig 2: OPC_UA VS OPC Classic

Fig 2: OPC_UA VS OPC Classic

In the end, the key feature that makes OPC_UA server the backbone for any IIOT system that uses PLCopen profile would be the fact that it allows customers to build extremely fast web/cloud base visualization even without a need to pay additional costs for licensing.

Fig 3 & Fig 4: Web/Cloud Visualization of data from monitoring a mini solar cell via OPC_UA

Photovoltaic Monitoring System With Visualisation – A Project with ITE College East

From |

Photovoltaic (PV) Monitoring System With Visualisation

The Photovoltaic (PV) monitoring system was designed to monitor the performance of the PV panels’ output versus the temperature on the PV panel. There were two different types of PV panels used for monitoring, namely the mono-crystalline and amorphous silicone (Thin Film). The data that was collected were the DC output and the temperature on the PV panels.

Continue reading →

Intelligent UPS Now Also Communicates with Higher-Level Controllers

From |

IQ technology turns Phoenix Contact’s Quint UPS-IQ power supply into an intelligent UPS for the mounting rail that provides continuous information about the charging state, remaining runtime, and lifespan of its energy storage devices, thus maximizing system availability.

The new data cable now allows the UPS module to be integrated directly into the automation application.

Continue reading →

Industrial PC Becomes a Control System

From |

Now, a standard industrial PC can handle any control task. The PC Worx RT Basic software PLC from Phoenix Contact transforms any industrial PC into a fully fledged control system. Programming, visualization, and control can therefore be combined in just one device.

Continue reading →