Tag Archives: HART multiplexer

Process Infrastructure – Ethernet HART Multiplexer

From |

Process infrastructure is one of the most critical parts of a refinery plant or offshore platform. The topology of modern process infrastructure includes FOUNDATION Fieldbus, Profibus PA, WirelessHart and HART Multiplexer etc.

HART (Highway Addressable Remote Transducer) is the most broadly supported protocol in the world for process industry as there are 40 Million HART devices being installed worldwide. But according to records, only 10% of these HART devices are connect to HART compatible control systems. End user should expand the use of HART devices in order to perform specialized operations like:

  • Asset Management
  • Predictive Maintenance
  • Data Logging
  • Partial-stroke Testing

Benefits of HART

Problems of Conventional Serial HART Multiplexers:

  • Slow scanning time due to large quantities of I/Os in the network
  • Limitation of RS485’s transmission speed
  • Work based on “Master and Slave” principle

Above are some of the challenges faced when using a conventional RS485 Hart Multiplexer and they will become worse if there are more than 1000 devices. Ethernet Multiplexer can solve this problem as featured below.

Fig 1: Ethernet Hart Multiplexer

Fig 1: Ethernet Hart Multiplexer

Ethernet Multiplexer Features and Benefits:

  • Works with existing standard IP infrastructure
  • Supports higher communication speed up to 1GB/s
  • Easy integration into Ethernet based Host system without additional conversion
  • Provides faster start up and device configuration
  • Flexibility in network design like redundant Ethernet
Fig 2: Hart IP Network Overview

Fig 2: Hart IP Network Overview

If you need any technical advice on your current project, feel free to contact us. I believe we can be your trusted partner to provide suitable solutions to fit your applications!

Ethernet HART Multiplexer – Transmit Process Data Via Ethernet

From |

Process plant with engineersDid you know that in the Process Industry, there are more than 40 million devices that are running on the HART Protocol and more than 75% of them are HART-enabled. However, up to 90% of these HART-enabled device are being under-utilized, used only to read the 4…20mA signal.

In the current trend of IIOT, there is a growing need for diagnostic data to be analyzed in order to reduce operating cost and increase system availability. The time from obtaining the diagnostic data to analyzing and determining the next course of action has to be almost instant.

In the past, if access to the HART data was needed, users typically installed an RS485 HART multiplexer connected to a PC. Whenever data from a particular field device is needed to be read, it can take a long time depending on the number of field devices connected to the RS485 HART multiplexer. This is because RS485 HART multiplexer works on a “master and slaves” principle.

Ethernet HART Multiplexer

HART Multiplexer

HART Multiplexer

Instead of using the RS485 HART multiplexer, Phoenix Contact introduced the Ethernet-based HART multiplexer. Our Ethernet HART multiplexer allows the user to easily parameterize and monitor field devices on the Ethernet network. The modular Ethernet HART multiplexer accesses other HART-enabled field devices using Ethernet-based fieldbuses such as PROFINET, Modbus/TCP, and HART IP.

Each device is an individual HART master which can be connected to higher-level, fast Ethernet network infrastructures. Up to 40 HART devices can be connected to existing configuration tools such as PACTware, Simatic PDM, Honeywell FDM, HART OPC server or HART server. End users therefore save time and costs since configuration and calibration, e.g. partial stroke test, process monitoring or current loop tests, are controlled via Ethernet and everything can be performed during active operation.

To find out more about Phoenix Contact’s HART Multiplexer, click here.