Tag Archives: ethernet switch

FL 2000 Managed Switch for Railway Applications

From |

Highspeed commuter trainFor many years, Phoenix Contact has been a reliable partner of the Railway Industry, supplying products such as Power Supply Unit, Terminal Blocks, Heavy Duty Connectors for railway applications. In the recent years, Phoenix Contact has invested a significant amount of effort to create innovative products such as controllers and ethernet switches for automation applications.

Ethernet-based communication medium/protocols are becoming the norm in modern automation environments. Traditional serial-based communication medium/protocols are unable to support the requirements for transmission speed and data size; especially for time-critical applications.

FL 2000 Managed Switch

Phoenix Contact's FL 2000 Managed SwitchThe new FL 2000 Managed Switch was officially launched in April 2017 during the Hannover Fair. This new series of Ethernet Switch was specifically developed to bridge the gap between simple unmanaged switches and complex managed switches which are already available within Phoenix Contact product portfolio.

In railway applications, data integrity is especially critical to ensure the smooth and safe operations of the system. Transmission distances from various subway station control systems to the main control center are often in the range of kilometers, which conventional copper-based medium cannot handle. The only way to transmit the data over long distance is via Fiber Optic technology.

Our sales team spotted an opportunity to propose our FL 2000 Switch in one of the railway system upgrading project in this region. We managed to overcome several challenges despite facing strong competitions from various industrial giants. The main unique selling points of our FL 2000 Switch that met with approval of the end user and system integrators were:

  • Feature important automation features with attractive price/performance ratio
  • Easy/Flexible Configuration/Setup
  • Comprehensive approvals to meet stringent industry-specific approval requirements
  • Various connection port options: Copper and Fiber Optics; Gigabit network possible

In addition, we are also able provide a bundle offer including our UPS and Power Supply Unit.

If you would like to find out more about our FL2000 switches, check out our website or you can leave us your contact and we will get in touch with you as soon as we can.

Ethernet Switch for Harsh Environments

From |

Phoenix Contact is now offering a five-port Ethernet switch with IP67 protection for use in harsh industrial environments. This switch sets itself apart as a result of the compact design and its ease of installation that makes it ideal for the machine construction sector. Its housing is only 30 mm wide so that it can be installed on a standard structural element completely and without any protrusion.

Continue reading