Tag Archives: automatic

CUTFOX 10 Automated Cutting Device

From |

Are you still using cutters to manually cut wires? Of course it would be practical if the job scale is small, involving less than 480 pieces of wire of length 0.5m daily.

What happens when you have a bigger job, where you are required to cut more than 1000 pieces of wire of length 0.5m every day?

One possible solution would be to buy another cutter to fulfil this requirement.

However, in doing so, you have an increased the labour cost to that of 2 well-trained operators.

Also, this does not account for human errors as well as quality issues. Are humans capable of repeatedly cutting wires of fixed length with an acceptable precision? Are they capable of running non-stop without tiring, constantly producing an output of virtually identical wires for extended periods of time? All of this would lead to increased costs and wasted materials.

With that in mind, what could cut wires with a consistent precision and can operate for long durations on end without rest? The answer is simple – a machine. Introducing Phoenix Contact’s CutFox 10.

Compared to the same range of automatic wire cutting tools in the market, our CutFox 10 has 2 additional functions with regards to its Speed & Software:

  • SPEED – Maximum Throughput of wire is 8mm with 0.5m/s max. feed rate.
  • SOFTWARE – CUTSOFT allows the CUTFOX 10 to read Microsoft Excel files, which can be exported to the machine. You can create a table of data with records of cutting jobs, containing information on the number of wires and length desired. These data records are then processed sequentially by the CUTFOX 10.

The Cutfox 10 not only cuts your labour costs, it also removes the costly element of human error and fatigue. In doing so, quality output is assured. In addition, it is also safe to use, compared to a manual cutter in the hands of a tired and weary operator, minimizing the risk of an accident.

This piece of automation ensures Return of Investment (ROI) in less than 6 months of constant usage, in addition to solving your manpower, quality and safety issues. If you are sick of cutting many, many wires, then this device is perfect for you!

If you are interested to find out more about our automatic cutting and crimping tools, feel free to contact us at marketing@phoenixcontact.com.sg!