Author Archives: randalchia

DIN Rail Plug-in Terminal Block

From |

Today I would like to share a bit on the little guy that usually goes unnoticed in our daily life.

The UMSTBVK Series – DIN Rail Mounted Plug-In Terminal Block

This product seemingly portrays images of an underdog. It has never been in the limelight by nature. That is due to the limited exposure that the UMSTBVK connectors are exposed to.

Other products such as the “UT 2,5/1P” Terminal Blocks & “UM 25” Interface Module are more commonly used in market, whereas the UT 2,5/1P terminal blocks are mainly used for high power feedthrough, and UM 25 interface modules are mainly used for signal feedthrough.

UT 2,5/1P

“UT 2,5/1P” Terminal Block

“UM 25” Interface Module

“UM 25” Interface Module

Comparing the trio, the UMSTBVK is actually a hybrid between the two.

Where are these products commonly used?

It is commonly used as a middleman between the controller and the field devices.  As the controller is usually the “Heart” of the entire system, hence, the use of UMSTBVK will come into place as one of the essential parts of the system, being “The Bridge” between the Controller and the field devices.

It will allow easy testing, maintenance and replacement for users, minimizing the need to connect and disconnect the wires that are already installed onto the main controller and field devices.

What are the most common objections as to using the UT 2,5/1P or the UM 25 modules integrated into their systems / devices / instruments?

  • Indeed these are convenient, but take up too much space.
  • Nice products, but pricing not very competitive.
  • Connectors for UT 2,5/1P has only one direction of wire entry, it compromises on the space taken in terms of depth.
  • There are no other options except 10 / 18 position for the UM25 Interface Module.

The UMSTBVK Series terminal blocks might not be the perfect solution, but it has the best features of both of its predecessors:

  • Great Versatility – Multiple variant of different number of position to choose from, and can be used on both NS35 / G DIN Rails.
  • Time-Saving – Minimizes time needed for assembly of terminal blocks into desired number of positions & eliminates the need to purchase additional accessory like “End Covers”
  • Readiness – “Clip and Go” type of product.
  • Cost Savings – competitive pricing based on per pole, which can achieve savings up to 30% per pole for the whole set including the plug in connectors.
  • Spoilt for Choice – You have multiple types of connectors that are compatible to choose from, with various connection technologies & angle of wire entry that you may prefer.
  • Screw Connection
  • IDC Connection
  • Push In connection
  • Crimp Connection

Up to this point, I see great potential for the UMSTBVK product family to shine in coming years.

Do you agree with me? If you do…

Do feel free to contact us at marketing@phoenixcontact.com.sg for more details to help you understand this better!

STRIKE – Leveraging on a Structured Sales Process

From |

I would like to share something I learned on a sales course I attended quite some time back hosted by a world renowned Tech Company, Hewlett Packard.

Although the course is mainly targeted at retail sales, we are able to relate some pointers back to corporate B2B sales.

STRIKE

The course is known as Sales STRIKE. Given the name of the course, in short, it shares a simple sales process that we can adopt.

“S” – Sell with Knowledge = Positioning / Key Selling Messages / Upsell

Knowledge is Power

(U.S. Defense Department graphic illustration by Jessica L. Tozer/Released)

Selling with knowledge is the first step to be taken by all sales personnel. It is a step of preparation for the sales personnel to know the products, solutions & market position.

Most importantly, selling without knowledge usually leave your customers a negative impression which will eventually increase the chances of losing the deal and this is definitely not the kind of impression i want to give to the customer. All Phoenix Contact sales representatives are trained with the relevant product knowledge within the first few months, and this includes me, which puts me at ease to sell a PxC product with confidence.

“T” – Tailor to Customers’ Needs = Ask the Right Questions.

Classic sewing machine

photo by: Uberprutser

This part of the STRIKE process is closely linked with the first step “S”. It means to understand your customers’ needs by engaging them with the right questions at the right time. Only then will you really know what they want. Customers these days are not only looking at your products; they are also expecting good service; someone who will understand them correctly. Customers are more likely to make a purchase when they feel that their needs are all being addressed by your solution offered.

Hence, identifying customers’ needs is all about asking the right questions @ the right time.

“R” – Recommend a relevant Solution = Good / Better / Best.

Porposal wooden tiles

Photo by: Nick Youngson (http://nyphotographic.com/)

Now that you have uncovered their needs, the next step is to provide a solution that fits their needs. Always go with an angle of benefits, not just features. And you will have opportunities to Up-sell at this point by providing a ‘Good’, ‘Better’ or ‘Best’ solution as sometimes, the solution that your clients choose initially may not answer their needs fully.

But many would ask, “How do you up-sell?” You can do so by following the basics below,

  • Understanding of the products
  • Always relate the up-sell to the customers’ needs you uncovered in the previous step.

Doing so, you will be able to raise your services to the level of ‘Solution Provider’, not just a product sales.

Remember, it’s the Benefits – Not the features!

“I” – Initiate a Demonstration = The “WOW Factor.

Singapore Black Knights Aerobatics team

Photo by Zexsen_Xie (https://commons.wikimedia.org/wiki/File:Black_Knight_Singapore_1_(12537881585).jpg)

It will come to a point where the right solution is proposed, but some customers will still be dancing Cha-Cha; being indecisive. That is most probably due to the missing “WOW” factor to give them the push they need to commit to the purchase.

Now, Initiating a demonstration to show them the solution you have proposed; to show them physically how it will address each need they are looking at, will help in creating a “WOW” factor for your customers.

“K” – Know how to close in any situation = How to handle Objections

Spartan Race

Photo by: Deveion acker (https://www.flickr.com/photos/draphotography/14750262951)

This portion of the process will be on how to handle objections which, on some occasions, may arise from opinions injected by a third party with no need for the solution or even from someone who does not even understand what you and your customer are working on. In most cases, these objections come from your customer’s own apprehension on some features or functions which they might not be sure whether it is critical to their work.

In such cases, what’s the best way to convince them again?
Lead them to answer their own questions. Provide relevant scenarios and pose those questions back to them for them to answer themselves. To which I will then say – “There you have it. You have answered your first questions yourself! Come let conclude this deal then….”

Now, this is a beneficial soft skill to gain by practicing and through experience. You can even try it out on your fellow colleague while convincing them to purchase a Watch / Phone / TV / Computer and you will realize it is actually quite a fun learning this process.

 

“E” – Explain the Need for Accessories

Euro

This final step in Strike is to cross-sell your services / add-on products that complement the solution you have already sold.

It can be a maintenance contract / accessories bundle that adds value to the solution even more.

Conclusion

These are just some simple lessons I have learnt that is helpful to me in my course of duties.

And I hope it does benefit everyone in some way or another that are reading this.

Happy Selling Everyone!

Let’s STRIKE !!!

You can contact:
Randal Chia
Mobile: +65 9223 4001 / Email: randalchia@phoenixcontact.com.sg