In the conventional method of data communication we often use wired systems. In the setting up of such systems involving data communication, we would need to plan the cable routes very carefully, and it is often very costly when the wires are required to be routed up and down such that obstacles are avoided in order to get connected. Usually the cost of the cables, labour, special tools for terminating etc. would be a considerably huge amount.

Besides the significant installation cost, physical degrading of the cable is a common issue faced (for example, wear and tear due to weather conditions, accidental cuts, scratches and bites by animals such as mice and ants). Especially when the system is down as a result of this, nobody would know which part of cable is broken or damaged.
In wireless technology, we could eliminate such worries and the less hardware used means that the risk of a breakdown would be lower. Aside from this, wireless technology has the following advantages:
- More flexibility
- Interference-free communication
- Mobility and freedom of movement of participants/devices.
- No wear and tear of the transmission medium
- Able to bridge long distances and problematic areas
- Neat looking
Applications of Wireless Techonology:

Some of our Industrial Wireless products are shown below:


An example of a typical setup:
Radioline Wireless Network


Wireless HART Network

Bluetooth Wireless Ethernet