Author Archives: John Tan

3 Key Reasons Why a Managed Switch Is Required in a Network Topology

From |

Most of us should know that there are 2 main categories of network switches, the Unmanaged Switch & the Managed Switch. However, sometimes we struggle to understand when to use a managed switch.

In this article, we will look at 3 key reasons why a managed switch is required in a network topology. Hopefully, after this, you can make use of these 3 key reasons to identify when a managed switch should be used.

Reason 1 – Building network redundancy

Not every type of network topology provides a redundancy mechanism. And what that means is that they will often have a single point of failure – where if one network switch fails, it will stop the entire network from working. Some examples of network topology without redundancy include Bus, Star and Tree etc.

To provide more than a single point of failure, network topology with redundancy mechanisms such as the Ring, Mesh and Hybrid must be used. Managed Switches can support such network topologies through different network protocols. Examples of the protocols include Media Redundancy Protocol (MRP), Rapid Spanning Tree Protocol (RSTP), etc.

Reason 2 – Acquire and provide data for network diagnostics

As Lord Kelvin puts it, “To measure is to know. If you cannot measure it, you cannot improve it.” Similarly, we need to know the diagnostic data of our network topology, to understand its status and improve it.

A Managed Switch provides important information that can help us to monitor the network topology and call for maintenance before full failure of the system happens. This could be classified as predictive maintenance, which brings great reliability benefits.

Some key diagnostic information includes:

  • Port connection status 
  • Redundancy connection status
  • Power supply status (Interruptions)  

The acquisition of these information could also be achieved through different automation protocols such as MODBUS, Profinet, Ethernet/IP etc.

Reason 3 – Security features

Managed switches offer security features such as user-interface & port security.

A user-interface security prevents any unauthorised access into the switch management and configuration. While port security allows only devices with a registered MAC-address to send and receive data packets through the network switches.

Summary

There are many other applications of Managed Switches, such as the use of Layer 3 & VLAN applications, which are critical for big networks. In Phoenix Contact, we provide a good range of network switches for different applications that you might have. Find out more in the following link or contact us at Phoenix Contact SEA.

Differences between ESD and F&G Safety Relays

From |

There are 2 main applications of safety relays in the process industry. Phoenix Contact describes them as the Emergency Shutdown (ESD), and Fire & Gas (F&G) applications. Across the industry, there are many terms used to describe these 2 applications. In this article, we will have a look at the different terms and understand the uniqueness of each application.

Application AApplication B
Emergency Shutdown (ESD)Fire & Gas (F&G)
De-energized To Safe (DTS)Energized To Safe (ETS)
De-energize To Trip (DTT)Energize To Trip (ETT)
Normally Energized (NE)Normally De-energized (ND)
Terms to describe the 2 applications

Emergency Shutdown Application

Under normal operating conditions, a load like an electrical motor, must be continuously powered. The ESD safety relay which is used to power up a load must also be continuously powered and is described as Normally Energized (NE).

During a safety incident (e.g. the electrical motor is overheated), the load needs to be switched off to achieve a safe state. As the power status of the safety relay and load has a direct relationship, switching off (de-energizing) an ESD safety relay, will result in the load being switched off as well. Thus, the terms, De-energized To Safe (DTS) and De-energize To Trip (DTT) are used to describe this phenomenon.

Example of ESD relay application drawing

Fire & Gas Application

Under normal operating conditions, a load like a sounder and a beacon is not powered. The F&G safety relay is only required to be powered up during a safety incident and to allow the sounders and beacons to sound off the alarm and provide light signals. Under normal operating conditions, the F&G safety relay is Normally De-energized (ND).

During a safety incident (e.g. a gas leak or fire incident), the load needs to be switched on to achieve a safe state. As the power status of the safety relay and load has a direct relationship, switching on (Energizing) an F&G safety relay will result in the load being switched on as well. Thus, the terms, Energized To Safe (ETS) and Energize To Trip (ETT) are used to describe this phenomenon.

Some people might be confused by the term, Energize To Trip (ETT). This is because the word “Trip” is commonly used on circuit breakers, where “Trip” here refers to power down. However, the word “Trip” has a deeper meaning and can be used to describe the powering up and down of a load. A similar word for “Trip” is “Trigger”, and you can think of it as “Energize To Trigger”.

Example of F&G relay application drawing

Summary

The key differences between the ESD and F&G safety relays are the type of load they are connected to, the definition of a safe state and the energy state under normal operating conditions. For ESD, the loads are usually machines used in production; the definition of the safe state is to switch off the relay / load and is normally energized under normal operating conditions. For F&G, the load are usually sounders and beacons, the definition of the safe state is to switch on the relay / load and is normally de-energized under normal operating conditions.

In Phoenix Contact, we provide smart solutions for functional safety, from non-contact safety switches to complex controllers. Our applications range from machine building, the automotive industry, and the process industry. Our products are also SIL certified, which allows you to meet your project requirements easily.

Example of PxC Functional Safety Products