Have you ever left your earphones in your pocket and when you wanted to use them again, they emerge as a tangled ball of mess? Annoying, isn’t it?

Well, the wiring of current and conventional electrical panels brings about a similar problem. The above picture shows its set up and at a glance, three words pop up in my mind: Complex; Costly; Time-consuming.
So why is this so?
Firstly, in the current system, multiple holes of different sizes need to be drilled in accordance with the cable sizes. Imagine the hassle having to drill ten holes of different diameter just to see messy wires intertwined together.
Next, a common occurrence to such wiring systems is the need to add additional cables. If you are lucky, there will be enough space on the flange plate to drill the extra holes. However, if the space is insufficient, or if you need larger holes for new cables, you would most likely have to replace the entire electrical panel and redo the entire wiring system from scratch. Not only does this add on to the hassle, it also adds on to labour and cost.
Lastly, conventional wiring systems require more time to rectify problems in communication. This is due to the difficulty in identifying specific cables especially when they are bundled together. The troubleshooting process thus leads to longer downtime which means financial losses for the company.
The Solution

Phoenix Contact has thus come up with a solution to eliminate this problem. Our Cable Entry System (CES) comes with specific features to tackle the hassle of the conventional system.
Firstly, only one or two holes would have to be cut to enable installation of up to ten cables in the system, greatly reducing the set up time. Furthermore, the CES can cater to different cable diameters ranging from 2mm-24mm. All these can be easily installed by mounting the sleeves of varying sizes on to the robust metal reinforced frame.
Next, additional cables can be installed by removing the blind sleeves from the extra cable holes provided by the CES. In the event that the existing cable configuration has to be amended, the CES allows for easy reassembly just by replacing the sleeves with those of different cable diameters. This eliminates the trouble of cutting out new holes on the flange plate.
Lastly, the CES allows cables to be easily identified as the rectangular frame organizes the sleeves holding the cables in an orderly manner that is easy on the eyes.
Besides tackling the inconveniences of the conventional electrical panel wiring, the CES offers protection class of IP54, making it suitable for harsh environment conditions.
If your current electrical wiring system reminds you of your ball of tangled earphones, it‘s about time you switch to Phoenix Contact’s Cable Entry System. Our CES will be the solution to increasing your productivity and cost saving to your electrical panels wiring.
Interested to find out more? Contact us at marketing@phoenixcontact.com.sg!