What are the differences between these power supplies and which one should you buy to suit your applications?
If you are looking for just a power supply…………..choose the UNO Power.
If you are looking for more than just a power supply with dynamic boost power reserve for reliable starting of difficult loads with 150% of the nominal current for 5 seconds………..choose the TRIO Power.
If you are looking for a power supply that can do more in terms of Comprehensive Diagnostics that enable reporting of critical operating states of the power supply before failures occur, LED display of the output power plus the option to enable the Magnetic Tripping of Circuit Breakers selectively via the Selective Fuse Breaking Technology (SFB) with 6 times the nominal current for 15ms……….choose the QUINT Power.
If you would like to know more about Phoenix Contact’s range of Power Supplies, Click here.