![]() |
![]() |
There are numerous smart relays in the market but PLC Logic is perhaps the only one that can have both control and monitoring capabilities while linked to an Apple iPad. This is done by using Bluetooth dongle, which turns the PLC Logic into a modern wireless control system. The range of Bluetooth devices is 100 meters with unobstructed line of sight and this translates to a lot of cost savings for applications that require control and monitoring remotely without the need to spend money for installation of communication devices and cable installation. The best thing is that the app is free from the Appstore. An additional plus point is that the interface looks really cool and clean, similar to what you can expect from an Apple Interface.
The PLC Logic also has versatile communication options to any higher level control system. It can support protocols such as PROFIBUS RS-232 RS-485 Modbus/TCP DeviceNet™ CANopen® PROFINET EtherNet/IP™ with just a change of gateway. With so many protocol options, there is no need to worry if the PLC Logic can support any higher level controller in the market.
One of the advantages PLC Logic has over the many smart relays in the market is that the relays are pluggable and replaceable. This solves the problem of the need to change the whole smart relay module in the event of a faulty relay. This translates to lower replacement cost. More importantly, downtime is greatly reduced and one just needs to change a relay instead of reprogramming the smart relay if the unfortunate relay gets faulty.
Another game changer in the smart relay market is that the analogue cards, both input and output, can be inserted as part of the main PLC Logic module without the need to attach a separate analogue module. This translates into cost savings as well as space savings. The analogue card supports both mA and V in full ranges. Besides that, there is also an analogue input card that supports PT100 or PT1000 sensor.
Last but not least, the PLC Logic comes with an option of full Push In connection technology. This can be found on the PLC Logic controller itself as well as all the corresponding relays that can be supported. The advantage of Push In is evident in applications that are prone to vibrations – you are well assured that none of the wires from the PLC Logic will be loosened.