FAQ About Radioline
Question: Which wireless technology is used in the Radioline devices?
Answer: A proprietary wireless protocol is used in the Radioline wireless system. The wireless technology is called Trusted Wireless and is specifically designed for the reliable transmission of data and signals over long distances. The new Version 2.0 offers adjustable data rates, encryption, extended diagnostics, and parallel operation of multiple networks.
Question: Is Trusted Wireless really suitable for industrial use?
Answer: The frequency hopping spread spectrum enables reliable data transmission even in industrial environments and in the event of interference.
Question: What range can be achieved with the Radioline wireless system?
Answer: Depending on the set data rate and the antenna used, the following ranges can be achieved with a line of sight:
- 4 GHz: up to 5 km
- 868 MHz: up to 20 km
- 900 MHz: up to 32 km
The above specifications is according to the product design, but sharing with you the test made in point to point configuration, having trees and structure as obstructions between two points.

At no line of sight, Radioline still transmits and receives analog and digital signals. Thus, Radioline works!