Phoenix Contact’s Contactron is a range of hybrid motor starters that is engineered and design to replace the traditional way of starting, stopping and managing the motor. And with that, it comes with numerous advantages and benefits to the system integrator, contractor and end user.
https://www.youtube.com/watch?v=Ap0iBA-BiqQ&t=63s
The most obvious advantage is the space savings it brings if one chooses to use Contactron instead of the using the usual contactors and thermal overload relay. The space savings can range from 50% to 89% depending on the motor configuration.
With space savings, one can design their panel or cabinet to be smaller. This is useful for sites where space is limited such as on top of a shipping port cranes. An even more remarkable savings can be achieved by using the Contactron to shrink the size of an Ex d explosion proof box by replacing the contactors and thermal overload relay.

Contactron setup compared to traditional motor starter setup
Secondly, the Contactron can very much reduce the downtime of a plant or factory as it can perform on average 10 times the typical service life of the traditional contactors. This is because, rather than depending on the ‘prone to failure’ nature of mechanical parts of the contactors, the Contactron uses a combination of solid state and electromechanical relay. Therefore, for motors that are subjected to frequent start stops, the Contactron is an obvious winner.
Besides that, the Contactron can be connected and communicated to a higher level control and monitoring system. This allows crucial information on statuses of the Contactron to be sent to the control system using common protocols such as Modbus, Profibus and Internet IP. This is crucial for visibility and productivity of the plant or factory operators. The traditional contactors with no intelligence have no possibility of being connected to a control system.
Besides, the above, there are many more advantages of using Phoenix Contact’s Contactron over traditional motor starters.
You can click here find out more about our Contactron Hybird motor starters
However, it will be best to be able to feel and learn about this with a face-to-face direct demonstration and presentation. If there is any interest, please feel free to leave us your contact at marketing@phoenixcontact.com.sg and we will arrange a visit to your office.