We are all available 24 hours a day. We have at least one cell phone, use the Internet on the go every day, and learn about the latest global news through our communication media. Having information at one’s fingertips is now essential to us all and nobody wants to give it up.
Think about the global competition in industrial production, which calls for us to continuously optimize our systems. As a production manager, you need to know at all times what is being produced worldwide on each machine, at what quality level and when the next maintenance interval is due. Such new systems are hardly imaginable today without efficient communication networks, which are essential for reliable system operation. This rapid development in the exchange of information and data that we have experienced in the telecommunications industry in the last few years is about to break into the industrial sector.
Indeed, many of these M2M (machine to machine) applications will be implemented over telecommunications networks. Now is the perfect time to consider these topics, applications, and technologies in the industrial sector.
Therefore I would like to share with you one of our success story implementing remote monitoring over the mobile phone network. The idea is to monitor remotely several paramaters on the oil well that is scattered in locations remotely using the GSM modem.
By doing this customer can get data more effective and efficiently compare to previously that one must go to every site locations and get information on the pressure and temperature at the oil well.
Solar-powered RTU
In this project we even integrate a solar system to power up the RTU and GSM modem since the location is remote and there is no power available. System architecture can be seen in the picture below:

Our GSM modem has a feature with dual sim cards which means when it detects low signal reception from one provider it can automatically transfer the communication to the other sim card. This is to maintain data availability.
We also set up a VPN tunneling in order to get a secure data transmission.
With this configuration, now customer is able to monitor oil wells data from office directly. They just need to select which location they want to monitor.
If you would like to know more on the remote communication using GSM modem, please do not hesitate to contact us. Thank you.