Terminal Blocks – Aren’t they all the same?

From |

When I visit Myanmar, customers would often ask me, “Why is it that Phoenix Contact’s Terminal Blocks considered a premium product?”

They will look at me, waiting for an answer, hoping that they did not say anything to offend.

“Aren’t all Terminal Blocks the same?”, after a brief moment of silence.

Well, the answer to this questions is definitely, no. They are not one and the same.

And that was how I sparked their curiosity. “Tell me more”, they said.

Look of disbelieve

The same look my Myanmar customers gave when they ask me about OUR terminal blocks

A Market Leader since 1923

I would go on and explained that the reason why Phoenix Contact has been the leader in such a simple yet sophisticated product, that today, it is trusted around the world.

So trusted, that projects in Southeast Asia, even big government projects, are using them.

If I have interest you, just like my Myanmar customers, then read on.

Meet the CLIPLINE complete – solutions for our Terminal Blocks

The CLIPLINE complete terminal block system gives you the possibility of responding flexibly to your customers’ requirements for all applications across the globe.

It comes in the following connections types:

  • UT universal screw connection
UT universal screw connection

UT universal screw connection

  • Simple PT push-in connection
Simple PT push-in connection

Simple PT push-in connection

  • ST compact spring-cage connection
Simple PT push-in connection

Simple PT push-in connection

  • QT fast QUICKON connection
QT fast QUICKON connection

QT fast QUICKON connection

  • RT robust bolt connection
RT robust bolt connection

RT robust bolt connection

  • Plug-in COMBI connection solutions
Plug-in COMBI connection solutions

Plug-in COMBI connection solutions

With up to 6 different connections, CLIPLINE complete terminal blocks offer screw, spring-cage, push-in, bolt, and plugin connections which enable you to react flexibly to the demands of your customers anywhere in the world.

Other than that, the CLIPLINE complete solution also boasts uniform accessories for all your connection needs:

Flexible jumper system

The same jumper could be used across our terminal blocks for all connection technologies.

To allow fast and individual potential distribution, the terminal blocks in the CLIPLINE complete system have two function shafts.

These are arranged in one line over all the terminal blocks, allowing for a combination of connection technologies.

Flexible jumper system

Flexible jumper system

Plug-in connection solutions

The COMBI connection system enables the time-saving and modular configuration of your application.

Like the terminal blocks, the COMBI connectors are available with screw, spring-cage, push-in, and fast connection technologies too.

The nominal data of up to 41 A and 1000 V have made a connection system for signal and power wiring possible.

The system meets the most stringent of vibration requirements. Both the terminal blocks and the plugs are touch proof.

Extensive accessories are available, from latching mechanisms to shield connections.

Plug-in connection solutions

Plug-in connection solutions

Large-surface marking

All the terminal points of the terminal blocks in the CLIPLINE complete system have large-surface marking options.

This is a precondition for clear wiring and startup and simplifies assignment during testing and maintenance work.

Optional large-surface snap-on marker carriers are available for group and terminal strip marking.

Large-surface marking

Large-surface marking

Standardized test system

 A comprehensive range of test accessories is available in the CLIPLINE complete system.

All test plugs make contact in the freely accessible function shaft. For individual measuring lines, a 2.3 mm diameter test plug is available.

More complex testing tasks can be implemented using alignable test plugs.

The corresponding spacers can be used to assemble individual test adapters perfectly suited for use in test laboratories.

Standardized test system

Standardized test system

Well, there’s more!

The above are just some features that make Phoenix Contact a market leader in terminal blocks.

If you watched our video below, you’ll understand why our CLIPLINE complete sets the competition apart.

So if you would like to find out more about Phoenix Contact terminal blocks, and you happened to be in Myanmar, give us a call.

We’ll give you all the answers you need and even provide samples of our famed terminal blocks.

Share

Share

Tell your friends about us!

Contact

Leave a Reply

Your email address will not be published. Required fields are marked *