A Wireless Solution – Easy Expansion Without the Hassle.

From |

Radioline – A Wireless Solution

What do you do when you need to collect more information from the field than you are currently able to? Traditionally, you would excavate then lay cables from the transmitter to the field device. A lot of hassle if your expansion was for just 4 signals. We may have just the wireless solution for you.

Recently, a water reclamation plant in the western part of Singapore had an existing system that required an expansion of 4 additional analog signal points. The distance between the field and the control room was only about 200 meters. However, to add just 4 signal from the field, proper wiring had to be done, including excavation and cable laying.

Our team, with the assistance of our system integrator met up with the customer to understand their needs. After determining the scope of work, a wireless solution was proposed. Instead of the labour-intensive cable solution, the team proposed the Phoenix Contact Trusted WirelessTM Radioline RAD-2400-IFS and the I/O extension module – RAD-AI4-IFS and RAD-AO4-IFS as an alternative.

Installing a wireless transmitter at both the field and the control room, our engineer then connected the analog signals to the IO cards, enabling the signal to be transmitted back securely. All this, from start to finish, we achieved in under an hour.

Trusted WirelessTM

Trusted WirelessTM 2.0 is a wireless technology specifically developed for industrial use. It provides rugged and reliable communications for your applications. In a 2.4 GHz band, Trusted WirelessTM 2.0 uses a Frequency Hopping Spread Specturm (FHSS) with up to 440 possible individual frequencies. Thus reducing the effects of interference signals.

radioline_solution

We not only saved our customer a significant amount of time and manpower with the Radioline Wireless solution, future expansions would only require the addition of IO modules.

If you are currently facing any issues and would like us to offer you our solutions, click here and send us the details and I will get back to you.

To find out more about Phoenix Contact’s Trusted WirelessTM Radioline, click here.

Share

Share

Tell your friends about us!

Contact