Sentosa is a popular island resort in Singapore , visited by some five million people a year. The attractions include a two-kilometre long sheltered beach, Fort Siloso , 2 golf courses, 2 five star hotel , a World class Casino in Resort World Casino and featuring the theme park from Universal Studio.
What does this have to do with Phoenix Contact?
Read more after the jump.
The island has an area of 5 squares kilometers. It lies half a Kilometers (a quarter of mile) away from the southern coast of main island of Singapore, with various recreation parks such as Golf Course and Fun Parks managed by the Sentosa Development Corp.
In order to remote monitor the pumps supplying water for long distances in the golf course, the pumps are equiped with our NANO Controller for remote monitoring purposes within the Golf Courses to trigger sms to respective person incharge in event of alarms generated from panels as well as pumps.
Product of choice:
The Nanoline GSM module uses a new approach, as the GSM modem is installed directly on the product and not via a serial connection with an external wireless module. This means that SMS messages can now be sent just as easily as sending text messages to an operator panel.
httpv://www.youtube.com/watch?v=m-Ax2zJ-Db4&playnext=1&list=PL009ED5DA4D818B9E