Case Study: PTT UT

From |

Southeast Asia’s oil and gas giant PTT from Thailand run their projects actively in Thailand Province “Rayong”. As PTT UT commonly build water treatment process plant along with their existing Oil and Gas plant. Electrical panels installed at site, commonly face with difficulty such as space limitation Therefore, all components installed must me space saving and yet reliable in functionality

In 2010, PTT UT  selected all control panel to be installed with Phoenix Contact Slim Type Relays at only 6,2mm in width that comes only with IP67 capabilities, as well as Phoenix Contact System Cabling that provide fast, faultless and unifrom wiring of I/Os signals to third party brand of PLCs.

PTT UT Choice from Phoenix Contact Includes:

PLC Relay:  a relay with high switching capacity with IP67 protections plugable relay.

System Cabling: A new front adapter that optimize housing design that provide space saving features, with faultless and uniform wiring of signals to the PLC

httpv://www.youtube.com/watch?v=a1zY-UaYf2g

Share

Share

Tell your friends about us!

Contact

Leave a Reply

Your email address will not be published. Required fields are marked *