Here is another IQ test for everyone. Again, this is a primary 6 Mathematics question. If it takes you more than “4 steps” to do it, then you have just complicate matters unnecessarily. I was “stunned’ by this question for more than an hour just to find a simple solution. Try it, give it a shot and post your answer in the comment box. ALL ARE WELCOME!
DIFFICULTY Level: 3 out of 5 Stars
QUESTION:
Runner X and Runner Y jogged to and fro repeatedly along a straight path between point A and B. Runner X jogged at a uniform speed of 4 M/s and Runner Y jogged at a uniform speed of 6 M/s. They started jogging from opposite direction at the same time as shown:
They first met one another at point P. The second time they met each other was at point Q. Given the distance between P and Q is 160M, Find the distance between A and B.

Answer: 400m
-Editor’s note: Working has been omitted out.-
Answer: 160m+160m+80m = 400m or 0.4km
800
400m
6AP = 4PB = 4S – 4AP
=> AP = 2/5S (1)
6S + 6QB = 4S + 4AQ = 4S + 4S – 4QB
=> QB = 1/5S (2)
S = AP + 160 + QB = 2/5S + 160 + 1/5S
=> S = (160 x 5)/2 = 400m
For those that have attempted and couldn’t get the answer, it is ok. The courage to attempt,is itself, the first step of a journey. Leave your ‘footprint’ behind by dropping a comment that you have attempted it. Then, come back and fight another day!
400
Spot this on blog browsing, kinda given a shot with primary 6 explanation:-
Given X’s speed = 4 m/s
Y’s speed = 6 m/s
and knowing Time = Distance/ Speed
At point P where X&Y meet, they spent same time of travel therefore:-
AP / 4 = BP / 6
AP = 4/6 BP (EQ 1)
Same goes to point Q they meet each other:-
(AP + BP + BP – 160)/4 = (AP + BP + AP +160)/6
AP = 4BP – 800 (EQ 2)
Solving EQ 1&2 get, AP = 160 and BP = 240
Total distance = AP + BP = 400m
Full mark???
Hi everyone, thank you for your participation. There is still more time before this contest is concluded, therefore, keep those answers coming!
Ans is 560m
If A to B is 0 to 100% and given the speed of runner x is 4m/s and runner y is 6m/s.
So the 1st meet point P is 40% of the distance of A to B.
with this same speed, the 2nd meeting point Q will be on the 3rd set of the run, where Runner x will reach B(100%) and back and runner y to A(0%) and back and it is 80% of the distance of A to B.
Given distsnce of P and Q (80% -40% = 40%) is 160m. so 100% is 400m
400m
Answer = 400 meter.
Answer will be released soon…
380
The test is closing! Any last minute entries? 😀