ImpulseCheck: Intelligent monitoring of surge protection

From |

Written by Dipl.-Phys. Claas Rittinghaus, Product Marketing Surge Protection, Business Unit Trabtech, Phoenix Contact GmbH & Co. KG, Blomberg, Germany

Condition Monitoring with ImpulseCheckProcess plant

Surge protective devices are safety-related components and, as such, an essential part of process plants. Information about the status and performance of these components as well as on the status of the plant itself play an important role in continuous monitoring and predictive maintenance. ImpulseCheck acquires all this information – and also enables it to be utilized in the Internet of Things.

The green “OK” notification on a typical status indicator of an SPD (Surge Protective Device), displayed on the device itself or read out by means of a remote indication contact, is not indicative of the current status of the arrester. Neither does it provide any information on the specific stress caused by surge currents and transient overvoltages since the installation of the SPD. Taking a look at the indicator during the maintenance or periodic inspection of a lightning protection system thus isn’t very meaningful. The surge protective system might fail just the next day – or in a few years’ time.

This is where ImpulseCheck, Phoenix Contact’s new system, comes into play. Surge currents and transient overvoltages discharged and limited by the SPD are detected in real time, and can then be analyzed in ImpulseAnalytics – a Proficloud application. In addition to comprehensive tools for the evaluation of the measured data, which are available to the user, the state of health (SoH) for each mode of protection is calculated for Phoenix Contact SPDs. The state of health is the current state of the arrester. As opposed to former, purely reactive replacements of surge protective equipment based on the green/red status indicator, this status information allows for the implementation of predictive maintenance plans. The efficiency of maintenance work can thus be improved, money can be saved, and system availability better protected.

Continue reading

Phoenix Contact Creates New Platforms, Alliances and Partnerships

From |

Digital transformation with Phoenix Contact

Phoenix Contact achieved sales of EUR 2.38 billion in 2018 with sales growth of 8%. At the same time, the number of employees increased to 17,400 worldwide.

“From a global perspective, we had very good growth figures in the markets, but had to accept negative currency effects,” says CEO Frank Stührenberg.” In Germany, still our most important market for Phoenix Contact, we again achieved a very good result with 7%. There was double-digit growth in all regions of the world”.

The company invested €207 million in IT infrastructure, machinery and equipment as well as buildings. An amount in excess of 200 million euros will again flow into investments this year. In China, for example, Nanjing, the headquarters of our Chinese subsidiary, will expand its production and logistics facilities to a total of 23,000 m². The location will be completely built according to Industry 4.0 standard. The site in France will invest 15 million euros in logistics and office space by 2020. The logistics in Harrisburg, USA, will be expanded by 7,700 m². A new building for printed circuit board connection technology with 10,300 m² is currently being built in Blomberg. Development units, laboratories and product management offices in the immediate vicinity of the production building will find their home here.

In the current year 2019, a budget of 7% of sales for research and development will primarily serve product technology for digital transformation as well as solutions for the future markets of energy, mobility and infrastructure.

At the Hannover Messe, which began on April 1, Phoenix Contact, once again, was the third largest exhibitor presenting its solutions for the digital transformation. With a total of 2,500 m², the company was present at 11 trade fair stands.

Learn more about our highlights and focal points at Hannover Messe.

Click here to know more about who we are and what we do.

Circuit breakers to protect your individual devices

From |

Narrow electronic circuit breakers – Universal at 6 mm

Narrow electronic circuit breakers – Universal at 6 mmIdeally suited for simple, space-saving potential distribution: the PTCB single-channel electronic circuit breaker can be bridged to the CLIPLINE complete terminal block system, and offers a setting range from 1 to 8 amperes with an exceptionally narrow overall width.

Your advantages

  • Simple application setup due to bridging option to CLIPLINE complete terminal block system.
  • More space in the control cabinet: narrowest protection with a width of just 6 mm.
  • Flexible use and a reduced inventory due to adjustable current values on each device for a wide range of applications.

Main features

  • Overall width: 6 mm
  • Operating state indicated via LED display in traffic light colors
    Fixed nominal current
  • Satisfies requirements in accordance with NEC Class 2
    Flexible use
  • Integrated remote signaling function

For more information, please download the flyer by clicking here or visit our website.

Visit us at Middle East Electricity 2019!

From |

Join Phoenix Contact Middle East

at Middle East Electricity 2019!

Middle East Electricity is the world’s leading trade event for the power industry. The show is split into five key sectors – power generation, transmission and distribution, lighting, solar, and energy storage and management solutions.

Visit for free and discover the thousands of power products and innovative technologies that are energizing the industry.

Live Hashtags

#MEE2019 #PxCMEE2019

 

 

VISIT US AT

STAND #H6.A10

Phoenix Contact, a global market leader and innovator in the field of electrical engineering, is headquartered in Germany. Phoenix Contact has five production sites in Germany and eleven abroad, with more than 50 sales subsidiaries and 40 representations. Its mission is to provide the best possible solution for your electrical engineering tasks. Phoenix Contact Middle East in the United Arab Emirates is an independent subsidiary with local management, sales, training, support and logistics operations. Their reliable presence in the region brings Phoenix Contact’s products and expertise into closer proximity to their clients and partners in the Middle East and Northeast Africa.

Post on Facebook or Twitter and use the hashtag #PXCMEE19 for a chance to win!

PHOENIX CONTACT Middle East FZ LLC

P.O. Box 345002, Dubai – U.A.E. | Office: 301, Block 10, Dubai International Academic City | Warehouse: PBU A11 and A12, Dubai Production City | Tel.: +971 4 437 0324 | Fax.: +971 4 437 0323 | Website: www.phoenixcontact.ae

Most popular topics of 2018

From |

Happy New Year!

Here we are uncovering to you the top rated topics and most read news of 2018!

In case you missed out on any of this, you now have another chance to read it.

Multi-level building installation terminal blocks with 10 mm² screw connection Multi-level terminal blocks for building installation save space

Our installation terminal blocks are impressing users with their low and compact design.

Read more

Overview of device circuit breakers Suitable for everyone

The complete portfolio of electronic circuit breakers provides intelligent protection for your power supply system. Take advantage of the easiest handling and simple product selection.

Read more

FDX 20 series splice boxesHigh speed, future proof data transmission

The new splice boxes from Phoenix Contact ensure continuously reliable data transmission in real time. With their compact, uniform design, the splice boxes ensure ample interior space for secure connection of fiber optics.

Read more

Apps for the PLCnext Control devices in the PLCnext Store PLCnext Technology – The platform for limitless automation

Enhance your automation thinking and discover the world of open automation with us.

Read more

TOPMARK NEOEfficient laser marker

The TOPMARK NEO laser marker redefines laser marking: with compact dimensions and easy operation via the integrated color touch display, it creates particularly robust and high-quality industrial markings.

Read more

Narrowest type 3 surge protection for 24 V nominal voltages – TERMITRAB The narrowest surge protection for I/Os and controllers

The narrowest pluggable device protection with an overall width of 6 mm, type 3 / Class III, with remote indication contact and Push-in connection technology. Also suitable for DC applications.

View product list

QUINT DC UPS for industrial networks QUINT DC UPS for industrial networks

The new Quint DC UPS uninterruptible power supply can be integrated into established networks and continues to supply your systems without interruption even in the event of a mains failure.

Read more

QUINT POWER below 100 W Compact high-performance power supply

For the first time, Phoenix Contact’s QUINT POWER power supply is offering superior system availability in the power range up to 100 W in a very small size.

Read more

 

People also read

Fast connection and safe supply
Intelligent groundwater abstraction
Space-saving potential distribution at a width of only 6 mm
Security with fine granularity for Modbus/TCP
Pick-off terminals for bolt terminal blocks with Push-in connection

Read all 2018 news releases

Press conference at the SPS IPC Drives 2018

From |

Phoenix Contact – Key partner on the road to a smarter world

Ulrich LeideckerUlrich Leidecker, President of the Business Area Industry Management and Automation, spoke at a press conference held at the SPS IPC Drives specialist automation trade fair in Nuremburg (November 27-29, 2018) about the positive development of the business situation, with sales for 2018 forecast to be more than € 2.3 billion by the end of the year.

Globally, the growth rates are good across all markets, even though there were negative currency effects in a large part of these markets. The Chinese market has continued to recover and, as in 2017, we are again experiencing double-digit growth. In the US, growth is slightly better at over 15 percent, but still slightly below the growth results of Europe, where – not including Germany – we have achieved 16 percent. With an almost 30 percent share of global sales, Germany is still the most important market for Phoenix Contact. A very good result is expected again for this market – this year with a growth of 7 to 8 percent. In total, the global growth is around 12 percent. Converted into euros, the nominal growth will be well above 8 percent.

The in-part turbulent market development – growth exceeded 20 percent in certain significant areas – has led to considerable challenges in the supply chain and in cost increases. We met this increasing development of sales by investing in all company divisions. We have therefore increased capacities significantly again this year: In Nanjing, China, the headquarters of our Chinese subsidiary, significant extensions across a total of 23,000 m² are being created in the areas of production and logistics. The facility will be built completely in accordance with the Industrie 4.0 standard. For the first time, large parts of the machine park and in particular the new logistics area will be completely automated with the PLCnext Technology controller solution. The total volume of investment in China in 2018 amounts to approximately € 30 million. The rapidly increasing demand in India requires a significant expansion of local production, the capacity of which has been practically doubled with the 2018 extensions. The total investment here amounts to approximately € 10 million.

Another focal point of the investments is the continuous expansion of the machine and plant park, which supports the opportunities of digitalization in our own company and translates the idea of “Industrie 4.0” into practical applications. From collaborative robots through to driverless transport systems, the latest technologies that support the consistency of digital value added chains and that increase efficiency in production are being used. The total sum of investments in 2018 will therefore amount to more than € 200 million.

As in previous years, our outlay for research and development is approximately seven percent of global sales. The total number of employees will have increased by approximately 1,400 to almost 17,500 in 2018. Without including acquisitions, the number of personnel in Germany will have increased by more than 500 employees.

Leidecker made a special point of mentioning that the largest acquisition in the history of the company so far would be completed on 2018-12-31. We have acquired the two companies SKS Kontakttechnik and Pulsotronic from the SKS Gruppe, a group of companies with whom we have been working in close cooperation for many years. The two companies will bring further technological and manufacturing expertise to the Phoenix Contact Group – and, naturally, will expand our production capacity. This acquisition will also increase the Phoenix Contact Group workforce by 400 employees.

PLCnext Store – Platform for software solutions

PLCNext Store Launched at SPS IPC Drives 2018

In order to be able to keep pace with the speed of technical developments, which is increasing significantly throughout the world, new approaches need to be found to harness existing knowledge on a broader basis. Against this backdrop, Phoenix Contact presented the PLCnext Store at this year’s SPS IPC Drives. This is a platform that makes it possible for all developers and market participants to offer self-developed software solutions and to purchase existing software solutions. For example, anyone who has developed a solution for pumping stations, lighting systems or driverless transport systems will be able to recoup their own expenses much more quickly by providing and selling this solution in the PLCnext Store. Those looking for suitable solutions or providers will be able to find what they are looking for much more quickly here in the future. The “App Store”, which is used so naturally in everyday life, is thus entering the industrial world. The idea of openness is of particular importance for market acceptance. Therefore, all providers – as well as competitors – will be able to place their software products for the PLCnext Technology controller solution on the market via the PLCnext Store.

Phoenix Contact in the midst of the Water and Wastewater Utility Revolution

From |

Phoenix Contact is in the midst of the increased awareness of the need and demand for new process engineering technologies, greater sustainability, smoother operation and in particular safety and security within the water management industry. Due to an increase in cyber-attacks, the issue of IT security has become a prime concern for operators of critical infrastructure.

Water and Wastewater Treatment

The Middle East and North Africa (MENA) region is facing major challenges in water sustainability due to a huge gap between supply and demand. In fact, many factors play a significant role in triggering these challenges such as demographic changes, climate change, the approach to micro-pollutants, and many other environmental and political issues that could lead to further water depletion and deterioration of the region’s stability.

As a reliable partner in this field, Phoenix Contact Middle East recognizes the most effective course of action to tackle these challenges. The company has been actively working with other industry leaders in the region to spread awareness and knowledge of the importance of adopting the right automation solutions for Water and Wastewater Treatment. During last October, Phoenix Contact Middle East held multiple seminars in the region in collaboration with other technology leaders in the field. The seminars held in the United Arab Emirates and Saudi Arabia shed light on the growing problem of water scarcity, and shared expert knowledge on water conservation and wastewater treatment by a high caliber of industry professionals.

Advanced system solutions for water supply and wastewater treatment are available at Phoenix Contact. The challenge now is to accelerate the adoption of these innovative solutions to enable a more sustainable management of the region’s water resources.

About Phoenix Contact

Phoenix Contact, a global market leader and innovator in the field of electrical engineering, is headquartered in Germany. Phoenix Contact has five production sites in Germany and eleven abroad, with more than 50 sales subsidiaries and 40 representations. Its mission is to provide the best possible solution for your electrical engineering tasks. Phoenix Contact Middle East in the United Arab Emirates is an independent subsidiary with local management, sales, training, support and logistics operations. Their reliable presence in the region brings Phoenix Contact’s products and expertise into closer proximity to their clients and partners in the Middle East and Northeast Africa.

For more information, please visit: www.phoenixcontact.ae

Phoenix Contact: Celebrating 10 Years

From |

Reflecting on 10 years of Phoenix Contact in the Middle East

Phoenix Contact 10th AnniversaryCelebrating 10 years of the establishment of our subsidiary in Dubai, being the first in our industry to establish a regional office, Phoenix Contact Middle East extends its sincere thanks to the leaders of the UAE and to all our business partners and valued customers in the region for their continued support, cooperation, and trust.

Phoenix Contact’s history has been shaped by a passion for innovation and technology. For generations, the firm has been committed to offering its customers the best quality in every respect. Phoenix Contact continues to invest in groundbreaking technology and in new products which will lead the industry in the upcoming times.

The firm’s approach is based on a solid foundation of trust and partnership. This motivates the company to take responsibility and gives it the needed freedom to come up with new ideas. In order to work together as closely as possible with their customers, they have established reliable local structures, supported by trusted channel partners to support their customers in their business wherever they are in the MENEA region.

Marwan Abdulaziz Janahi, Managing Director of Dubai Science Park, said: “Phoenix Contact was one of the very first businesses to establish in Dubai Science Park, and has since played an integral and pioneering role in developing our vibrant community of more than 350 companies and 3,600 industry professionals. It is with pride to have witnessed Phoenix Contact grow from strength to strength, as it is our mandate to support our partners. We wish Phoenix Contact our heartiest congratulations on journeying with us for the past 10 years.”

Surge protection training course

From |

Interested to learn more about the phenomenon of surges and how a surge protection device works?

Then this training is tailored to your needs

Surge protection training

We are pleased to announce that we are holding a one day training course on Surge protection on the 21st October, 2018 at the Phoenix Contact Training Center in Dubai, located at the Dubai International Academic City. You are invited to register for this training and invite your colleagues/ friends to register as well.

Developed and conducted by an expert in this field, Mr. Eugen Friesen – Strategic Market Support at the Business Unit TrabTech – Phoenix Contact GmbH & Co KG -, this comprehensive training course aims at enhancing your understanding of surges and the functioning of surge protection devices.

Upon successful completion, all participants will be issued with a Certificate from Phoenix Contact.

Click to register

 

 

 

 

Phoenix Contact Solar Park Management

From |

Solar Park management: automation and networking

Operarte photovoltaic systems efficientlyPhotovoltaic (PV) systems have become an important and established source of power, with a current installed capacity of approximately 230 gigawatts worldwide. In the Middle East alone, 11 gigawatts projects have been announced that are either in the bidding or the pre-qualification stage. The main driver for adopting solar and renewables in the region is the low prices of solar energy that led policy makers and industry leaders to take a number of steps towards increasing and accelerating the adoption of it.

Photovoltaic systems are being installed in industrial areas and public spaces more and more frequently because environmentally friendly power sources are perceived positively by the public. This trend is further fueled by the fact that PV applications are easy to use.

Continuously record and evaluate all data from the photovoltaic system First of all, to enhance the efficiency and yield of your photovoltaic system, you need to use a continuous operating data acquisition and intelligent data management. Irrespective of which transmission medium you use, Phoenix Contact has the right network components for you to set up a failsafe communication solution. The basis for this includes the high-performance Gigabit switches, modems, and media converters.

Moreover, the profitable operation of large photovoltaic systems requires continuous monitoring and control at segment level. The Array Control switchgear and controlgear assembly from Phoenix Contact performs this function and records all relevant data related to the current performance of the arrays, the ambient conditions, and the inverter status. This data is transmitted to a higher-level SCADA system in the central control room.

Phoenix Contact provides standard and customer-specific solutions for the automation and visualization of photovoltaic systems. Read more