Digitalization has made its way into power generation plants and substations, thus, creating a new challenge for system planners. With this new challenge comes high volumes of data that needs to be transferred from central to remote stations. These stations are often located in harsh environments.
System planners typically use copper cables at power generation plants and electrical substations. However, with digitalization, the data volumes reach to an extent that copper cables cannot handle. System planners are therefore switching to Fiber Optic (FO) cabling systems. The FO cables are 90 percent lighter and thinner – allowing for longer transmission paths and higher data rates.
Planning a FO cabling system is a complicated process involving complex implementation. From selecting the right connection technology to the corresponding tools. Trained specialist personnel need to select the right equipment for this technology and for the field assembly.
Time is money! Hiring a specialist personnel from a specialist company is time consuming. In this case, your own personnel can use a Plug and Play system to do the same job – without tools. Working in such harsh environments, also require a high degree of protection for connection components, such as IP67.
Components for different configuration levels
The M17 circular connector is the centerpiece of Fiber Optic cabling systems, available with 4 to 24 positions.
The 12- and 24-pos. connecting cables with M17 MPO connectors are ideal for cabling paths. They are available in different lengths and installed in underground conduits and cable ducts. With the factory-assembled connectors, they can provide direct connection between cabinets.
Moreover, to enable the variable connection of the M17 cables to the end points, different versions of distribution panels are there. They provide the transition from the robust IP67 world to the IP20 world and its active components.
Fiberglass for data transmission
System planners can now use a special multi-mode fiberglass in FO cabling, hence, allowing transmission of data rates up to the Gigabit range covering distances of 100 meters.
For reliable transmission at data rates up to 1 Gbps over long distances of up to 300 meters, the M17 FO cabling system has been equipped with proven multimode optical fibers. Accordingly, meeting the requirements for an OM1 fiber and key international standards.