Footprints of Lightning Strikes

Lightning strikes in systems
Lightning strikes may cause devastating damage to buildings and facilities. Depending on the energy, there is massive destruction or damage, which may cause not so obvious, yet consequential cumulative destruction. Lastly, additional risk persists for high, large or exposed located structures.
The Lightning Monitoring System LM-S from Phoenix Contact captures lightning strikes and also analyzes the peak current, specific energy and charge of lightning surge currents. It consists of sensors for the down conductors of a lightning protection system and the analyzer. This data is easily accessible via the integrated web interface at any time from any place. It provides lightning strike information of the facility and enables preventive maintenance. Based on data from the LM-S system, measures take place quickly in order to avoid consequential damage and downtime. Taking this into consideration, maintenance or service work will be unnecessary as long as the effect is noncritical.
In structures that are not significantly prone to but have lightning-related sites, LM-S comes in handy for lightning research.
Phoenix Contact Lightning Monitoring System is installed on world-famous buildings such as Burj Khalifa.
Click here for more information about our LM-S system.

Hand tools and automatic devices have become essential for conductor pretreatment in the day-to-day workflow of manufacturing companies (across all industries). High-quality components contribute to Phoenix Contact’s tools, hence provide you with:
The ISA UAE Automation Conference and Exhibition 2016 is a full-scale conference and exhibition in the Gulf Region dedicated for process automation and will be held to emphasize on the local content and to reflect the true position of UAE as a major market of automation products and technologies.