Speed Starters for Asynchronous Motors

From |
Asynchronous Motor

Asynchronous motors are supplied via over-dimensioned frequency converters (FCs). Since a speed starter’s noteworthy advantages include quick installation and starting, it is perfect for simple programs with few functionality.

Industrial plants contain a large number of electric motors. The majority of motors carry out straightforward functions, such as moving things or liquids from one location to another or carrying out the necessary processes.

Speed Starter Steps

Logistics centers, machines, and systems perform these tasks. A motor is operated in a variety of ways. Nowadays, frequency converters are employed in the majority of applications, particularly when soft starts or varied speeds are necessary.

Frequency converters are intricate machines that perform several tasks but are frequently oversized. This is due to the fact that their most prevalent applications at the moment usually include straightforward activities that simply demand for two fixed speeds and/or a ramp function with a gentle start and soft stop of the motor.

Safe shutdown up to SIL 3 and PLE

A device class between motor starters and frequency converters is provided by the new speed starter from the Contactron product family. The small solution provides all required features in a single housing and impresses with its simple operation:

The CrossPowerSystem power distribution system
  • Direct start of asynchronous motors
  • Reversing start
  • Full motor protection
  • Different speed settings
  • Soft start and soft stop of the motor
  • Safe stop with Safe Torque Off

The device has several benefits for the user, but its built-in Safe Torque Off (STO) capability allows for a safe shutdown up to safety levels SIL 3, PL e, and Cat 4. There is a substantial space savings in the control cabinet due to the small housing dimensions, which have an overall width of only 35 millimeters.

Easy wiring and an intuitive operation concept ensure quick installation and startup. As a consequence, it is possible to adopt a cost-effective solution using the speed starter from the Contactron product family, which has all the essential features for varying speeds and soft start.

In the most common uses, an emergency stop switch must be able to securely stop rotating and moving parts, for instance, in the event of a jam or an emergency. Use the Contractron series’ quick starter to design a redundant system and prevent malfunction, hence, ensuring safety.

Therefore, a second contactor is not necessary for a safe motor shutdown. On the controller side, use the STO+ and STO- connectors to accomplish a two-channel shutdown . With only a short installation area, the Contractron fast starter achieves safety classifications SIL 3, PL e, and Cat. 4.

Quick startup in less than a minute

Machine manufacturer can offer a more competitive solution and speedup the application installation by using Phoenix Contact’s speed starters.

To start the motor and apply a control signal to an adjustable fixed speed, you must wire the load input and output. The motor can then start operating right away. It must be possible to customize the parameters for the appropriate application, of course. The user-friendly operating idea, which consists of a display, five LEDs, two up and down buttons, a set/reset button, and a rotary switch, accomplishes this.

Setting the motor’s nominal current is the first step in protecting it against overload. As a result, it is no longer essential to install an additional motor protection relay. Set the rotary switch to the “Current” position and input the desired value by using the up and down buttons. Verify the value by pushing the set/reset button. When a value is changed, it immediately begins to flash in the display. The value is always visible after saving. It is also simple to adjust the ramp time, or the amount of time the motor takes to reach the desired speed.

To achieve this, the user simply moves the rotary switch to the “Ramp” position, inputs the new value using the up or down button as previously mentioned, and saves it by pushing the set/reset button.

Different versions for different requirements

speed starter operator interface

Set the rotary switch to “Status” to view electrical values such as frequency, current, voltage, temperature, etc. Use the same method to adjust the speed.

Set the speed to the “Speed1” position and select the correct frequency value by using the up and down buttons. Verify your selection by pushing the set/reset button.

The LEDs flash in the “R” or “L” direction of rotation, which is also selectable with the up or down button and remembered by pressing the set/reset button. Repeat this procedure to facilitate a second speed:

  1. Move the rotary switch to the “Speed2” position.
  2. Specify the value using the up or down button.
  3. Press the set/reset button to confirm.

If desired, the user can make additional settings by turning the rotary switch to the “Options” position.

For single-phase and three-phase load input, the speed starters of the Contactron series offers performance classes ranging from 0.25 to 1.5 kilowatts, with or without an integrated EMC filter. The devices with filters built in come with a plug-in, changeable fan, whereas the ones without filters only have a heatsink.

In conclusion, fast starters are a convenient option appropriate for a variety of uses. Users gain from a device class positioned between motor starters and frequency converters under the tagline “Connect, set, start.”

M17 Fiber-Optic Cabling System

From |

Digitalization has made its way into power generation plants and substations, thus, creating a new challenge for system planners. With this new challenge comes high volumes of data that needs to be transferred from central to remote stations. These stations are often located in harsh environments.

System planners typically use copper cables at power generation plants and electrical substations. However, with digitalization, the data volumes reach to an extent that copper cables cannot handle. System planners are therefore switching to Fiber Optic (FO) cabling systems. The FO cables are 90 percent lighter and thinner – allowing for longer transmission paths and higher data rates.

Planning a FO cabling system is a complicated process involving complex implementation. From selecting the right connection technology to the corresponding tools. Trained specialist personnel need to select the right equipment for this technology and for the field assembly.

Time is money! Hiring a specialist personnel from a specialist company is time consuming. In this case, your own personnel can use a Plug and Play system to do the same job – without tools. Working in such harsh environments, also require a high degree of protection for connection components, such as IP67.

Phoenix Contact offers the perfect solution combining the strengths of the M17 circular connector with those of a FO infrastructure.

Continue reading

Phoenix Contact’s Trio Power Supply

From |

Application-compatible power supply are necessary for a future-oriented infrastructure, whether it be for telecommunications or train technology. With an input voltage range of 230 V AC to 400 V DC, the new Trio Power power supply offers a high-power density, parallel mode, and a highly durable electrical and mechanical architecture. As a result, it completes Phoenix Contact’s extensive line of power products and is perfect for infrastructure transitions, such as those in train technology.

Digital signal towers: new decentralized structure for railway technology.

Denmark, Norway, Germany, and other nations have decided to digitalize their railroads in order to advance the development of the European Train Control System (ETCS) and digital control tower technology. Along with further network extension and the employment of cutting-edge technologies, digitization is a crucial component in modernizing the rail system and, more importantly, in boosting performance.

German trains will need to adapt for a digital future, moving from traditional signal technology to radio-controlled train operation and utilizing cutting-edge technologies like artificial intelligence. Such technologies will enable fully automated train operation, real-time control, and accurate location in the future. Deutsche Bahn and the German Railway Industry Association established this industry wide Digitale Schiene Deutschland (Digital Tracks in Germany) program to accomplish this.

It is vital to upgrade not just the systems themselves but also the infrastructure, control, and safety technology in order for the digital technologies to coexist peacefully. By 2035, the integrated command and control system (iLBS), digital control towers (DSTW), and the full rollout of the ETCS will have completed this fundamental reform.

Increased capacity, optimal use of the rail network, and the change of transportation will all be significantly aided by modernization.

Obstacles to implementing railway technology

It is significant to remember that the components for railway technology are subject to tremendous stress in addition to the technological and structural constraints. Particularly when it comes to solutions for switch, signal, and barrier management as well as communication technologies close to the track, a sturdy component design is crucial.

Why do power supply in control cabinets near to railroad tracks need to be so strong? High needs are brought on by harsh climatic factors including extreme heat or cold, dampness, and dust. A high level of interference and vibration resistance is also required due to the high voltages and vibrations near the control cabinets. Long service life and a compact, low-maintenance design are further prerequisites for success in railway technology applications. It is necessary to adhere to the applicable criteria.

The design of systems and infrastructure in German railway technology focusses on telecommunications technology. In the future, 48 V will replace the 24 V operating voltage currently used for controllers—such as for switch controls and an extra 48 V voltage level—as the typical main voltage.

Trio Power Supply: Robust and reliable

Phoenix Contact’s Trio Power power supply exceeds exacting standards and was created primarily for use in infrastructure applications. The new power supply is ideal for use in these applications due to its shock and vibration resistance and sturdy mechanical and electrical architecture. Use the IEC 60068-2-64 standard and the railway-specific DIN EN 50125-3 standard to measure the equipment’s vibration resistance. This indicates that the equipment functions dependably even when traveling very quickly.

The new power supplies’ wide temperature range allows for a significant degree of flexibility in terms of potential applications. When exposed to temperatures between -25 and +70 °C, the power supply units are dependable and produce high power.

The Trio Power power supply has strong mechanical components as well as dependable and enduring electronics. The result is that the devices are input-side voltage-proof up to 300 V AC and 420 V DC. Another safety feature is overvoltage protection VP (OVP), which restricts overvoltage to 58 V DC. Furthermore, use control card with a protective lacquer covering to use the devices on 48 V applications subjected to heard weather conditions.

Use Trio Power supply in numerous supply networks worldwide as they come complete with an AC and DC wide-range input.

The power supply contain a dynamic power reserve that allows them to start heavy loads with reliability. For up to five seconds, they provide 1.5 times the nominal current. They also guarantee a high level of energy efficiency due to their high efficiency rating. Link multiple power supplies to generate more power. The devices’ enhanced load distribution allows for parallel operation for increased power and redundancy. Reduced inrush current improves availability even more and makes primary protection much simpler.

Challenges in telecommunications and infrastructure technology

Numerous applications, including artificial intelligence (AI), autonomous driving (Car2x communication), and intelligent production (Industry 4.0) need a quick, efficient, and secure infrastructure.

The existing 5G technology is being expanded to deliver this, and the follow-up technology is already off to a start.

The pressures on technology and systems are increasing as mobile data traffic between smart devices gets faster and more intense. Design network and communication technologies for infrastructure in order to be future proof.

Autonomous driving illustrates these connections. Share maximum amounts of data in real time between the vehicles and the transportation infrastructure to reduce traffic accidents Communication systems need powerful computers and operate at rapid rates to transmit and assess data.

The forthcoming 6G technology will have exceptionally fast data rates, albeit at the expense of transmission distance. The terahertz waves utilized for 6G also have wave properties that are more similar to infrared light than microwaves. The likelihood of redirected and obstructed waves passing through objects increases, particularly in urban settings. Future infrastructures will need numerous sending and receiving technologies to handle these issues.

Ensure a compact, maintenance-free, and environment-proof power source, such as a Phoenix Contact’s Trio Power with a wide input voltage range and 48 V DC voltage by using a dependable power supply on these decentralized systems, such as radio masts and transmitting and receiving systems.

PLCnext Technology in Water and Wastewater applications

From |

Water and wastewater applications and PLCnext Technology

“With increasing awareness of climate change and sustainability in society, the focus is increasingly turning to water management. New challenges such as falling water table levels, increasing pollution, micro-plastics, and increasing storms are causing an increase in requirements. Solutions from Phoenix Contact are increasing the level of transparency, efficiency, and resource conservation.”

Phoenix Contact develops automation, communication, and remote control technologies for all forms of water treatment plants and wastewater treatment plants. From the control room, through the network and control level, all the way to the field devices and machines. Our customer-specific and ready-to-use solutions are based on an open system and open interfaces that guarantee future-readiness.

Automation of a waterworks and wastewater treatment plants, require new levels of transparency and efficiency for these processes. Furthermore the automation is necessary to meet the requirements of future challenges of a digitalized world.

PLCnext Technology as a basis for solutions in the water and wastewater sector

PLCnext Solution App – PumpStation Control

Application

Pumping stations are mostly de-central facilities including pumps and equipment for pumping fluids from one place to another. A variety of infrastructure systems, use them while equipped with electrical instrumentation to detect the level of wasterwater. These include canal water supply, drainage of deeper areas, and wastewater disposal from processing plants. When the wastewater level in the shaft rises to a pre-defined level, the pump starts lifting the wasterwater up in a sewage system.

Solution idea

Ready-to-use solution app to control and monitor a typical pumping station with up to three pumps. You can download the app from the PLCnext Store and download it directly to a PLCnext Control. The PLCnext Control uses standardized I/O modules and interfaces to collect the data from the field level. The app contains industry-specific functions. You can set the parameters via the integrated PLCnext eHMI. The eHMI also visualizes all important information about the pumping station. The integrated Proficloud interface transmits all important information, alarms and operating data to a dashboard or to the customers’ scada system. In addition, you can send all data directly to the customer’s scada system via OPC UA. Read more…

Water Functions – the process library
for water management

Application

Water management technologies and procedures are constantly being developed and adapted. Due to the changing conditions, process systems are subject to a continuous process of change.

This requires existing systems to be optimized and adapted in order to ensure the best possible supply and cost-effectiveness for operations. With a modern and efficient solution, you will meet these these challenges.

Solution

Water Functions, the process library for water management, enables you to ensure the efficient engineering of your systems based on preprogrammed function blocks. The library contents range from a basic function for the simplest applications to complex drive, valve, and measurement blocks as well as blocks for connection to a SCADA system. Water Functions includes function block and HMI libraries for PLCnext Engineer which supplement the PLCnext Technology from Phoenix Contact with useful functions for the water and wastewater treatment. The Water Functions libraries are the continuation of the old Waterworx library on the classic system with many useful functions such as regulation, control of field devices like motors and valves and many others for process automation.

A wide range of technologies, such as PROFIBUS, PROFINET, Modbus, and OPC UA, allow the user to integrate new and existing field devices into the overall system without any problems. Thanks to close cooperation with manufacturers of typical field devices for the water management industry, the user is able to integrate field devices in an efficient, verified manner.

Thanks to the continuous further development of the Water Functions process library, the number of possible connections is constantly growing.

Join our live webinar on Tuesday 6th April to find out more and learn how our sophisticated system solutions for water supply and wastewater treatment, can help you reach your goal of sustainable market success and experience long-term success.

For more information, please contact Pradeep Menon at pmenon@phoenixcontact.com.

Phoenix Contact stands up to the Corona trend – Digital press conference on the occasion of SPS connect

From |

At Phoenix Contact’s annual press conference in November, Ulrich Leidecker, Chief Operation Officer, spoke about the company’s economic development, which will be better than could be expected at the beginning of the pandemic.

Ulrich Leidecker

From today’s perspective, Phoenix Contact will close the financial year 2020 with a moderate sales decline of -4 to -5 percent. Excluding currency impacts, the rate will be around -3 to -4 percent. That is a very good figure for this industry. From a global perspective, we are experiencing an uneven level. The Americas are in the double-digit minus range, while Asia has been developing very positively since September with an increase in incoming orders. China is showing a sales growth of over ten percent, and the growth curve in the USA is also slowly rising again.

We continued to make significant investments even in 2020, the year of the coronavirus. A total of around 150 million euros will be invested in new structures and innovations. In Nanjing, China, a building complex at a second location near the airport is nearing completion. About ten kilometers away, a new production building with its own logistics facilities of around 34,000 m² of floor space has been built in Mozhou, Nanjing’s newly developed industrial area. A housing complex for employees was also built. Together with a company restaurant, this adds an additional 7,750 m². Phoenix Contact has also invested in Russia and is now part of Europe’s largest technology park in Skolkovo, with 2.6 million m² of space. Here, industrial companies, research laboratories, start-ups, and a university offer a unique high-tech combination.

At the Blomberg site, the logistics unit was expanded while operations continued. Nine additional shelving aisles now offer 64,000 new storage spaces. The additional workstations will increase order picking performance by up to 40 percent. The investment amounts to 15 million euros.

With an investment of 6 million euros, the new logistics building in Herrenberg was completed in the first quarter of 2020. At 2,900 m², the new facilities provide an automated small parts warehouse (AKL) and a pallet rack warehouse. The relocation of the warehouse allows production to be expanded into the space previously occupied by logistics. Phoenix Contact E-Mobility has also further expanded its production capacities. In Germany, a new production area of 5000 m² is being occupied. In addition, a new production plant with an area of 15,000 m² is being built in Poland. Corporate spending on research and development is more than seven percent and has continued to increase slightly compared to 2019. The number of employees worldwide will be around 17,500 in 2020, unchanged from 2019.

Empowering an All Electric Society

All Electric Society - Phoenix Contact

The described activities in all company divisions all serve the goal of making Phoenix Contact an essential partner in a challenging future. We tie our future as a company to the global prospect of sustainable energy production. Climate change, reducing the levels of CO2, the growing world population, and a predicted doubling of the world’s energy demands by 2050 ‒ to meet these challenges, doing without and refraining from things are not enough. New technological approaches are needed. We believe that the world is indeed facing an energy revolution that will usher in the end of the fossil fuel age: A society whose entire energy demands are covered by electricity generated from renewable sources, a completely CO2-free energy supply. This vision has the potential of eliminating the unavailability of energy as one of the world’s most important barriers to economic development, without destroying our natural resources in this endeavor. For years, we have been supporting our customers in areas such as energy efficiency or furthering renewable power generation systems by expanding them and connecting them to the grid. In factory automation and infrastructure, we help with the electrification, networking, and automation of essential structural and production-related elements. We need to expand these efforts greatly in the coming years if the vision of a world powered by a renewable energy supply is to become reality. Additional important aspects will arise, though:

One of the decisive factors will be what is known as sector coupling. We must ensure that the network combines all the energy-generating, consuming, and storing sectors of industry and business as well as of private households and municipal areas. Surplus energy must be stored. This means through conventional means or, in the future, through more “Power-to-X” applications in which hydrogen is produced and stored by means of electrical energy through water electrolysis, which can be converted back into heat or electrical energy by fuel cells or traditional generators when energy requirements increase. In the same way, the hydrogen could be further processed into “green fuels” to serve as regenerative fuel for aircraft. Networked solutions help to bring surplus energy generated at one location to the places where it is currently needed. And this is exactly where we see our contribution as a company. With our solutions, we can contribute to solving major global and social problems and, at the same time, participate in economic development.

Mechanical products such as terminal blocks form the basis for the electrification of industries – the starting point of Phoenix Contact’s corporate development. Thanks to digital item descriptions, these terminal blocks can be efficiently integrated into planning and engineering tools. This is one of the basic prerequisites for the digitization and automation of systems. This is how terminal blocks also make the industries smart.

New communication technologies such as 5G, SPE, and TSN form the basis for the intelligent networking of industries. Using these technologies is the only way to ensure that data points in various sectors can be networked securely, simply, and quickly. We develop all these technologies further and apply them.

Phoenix Contact’s vertical market management aims at developing applications and using them to benefit an All Electric Society. It also benefits factory automation, where the long formulated demand for Industry 4.0 has been described in principle, but is far from being used in daily industrial operations. In the vast infrastructure segment, ranging from smart buildings to smart cities and all forms of smart traffic, there is still a long way to go. This is especially true for sector coupling, which describes how forms of energy can be exchanged efficiently and combined among the individual sectors. Examples range from simple ones, such as combining solar power and electric storage or electrically powered vehicles, up to power-to-gas offshore platforms that convert wind power into hydrogen on site and distribute the energy via pipeline or store it as liquefied gas. This brings us to a rapidly changing world of process technology. In addition to efficiency and modularization issues in the chemicals and pharmaceuticals sector, the oil & gas sector will certainly see the most significant changes. The major oil companies have long understood this and are resolutely moving to alternative strategies for producing and distributing energy. There is also a high demand for electrification, networking, and automation for completely new applications in this sector. This also applies to the energy sector, of course. A changing energy production also needs new structures and processes for distributing and storing energy. Today’s networks are designed so that energy is generated at comparatively few points (power stations), fed into the transport network at high and extra-high voltage, converted to medium voltage, and then distributed further in the distribution grid. After the energy is further converted to low voltage, the actual consumers are supplied by secondary substations. But what if more and more consumers also become producers? What if more and more wind parks and solar parks feed in at the medium-voltage level, where until now energy was “just” distributed? In short, the demands for expanding the energy network will be great and Phoenix Contact will lend support with an ever-growing range of services and applications as a solution partner.

For more information, please visit our website.

Global prosperity through an All Electric Society

From |

To keep up with today’s world’s needs, we need to adapt to constantly changing needs and offer the best solutions that meet those needs. Today’s world is full of challenges that also offer new opportunities.

Phoenix Contact’s vision is to become a reason and part of a sustainable and climate-friendly future.

The All Electric Society

The All Electric Society is a concept based on research findings from scientists and engineers from universities, institutions and companies all over the world. In a joint video keynote, CEO Frank Stührenberg and CTO Roland Bent explained what lies behind it with a look back into the past of why Phoenix Contact is the ideal partner for this journey into the future. “The success of Phoenix Contact is based on the fact that we have always provided suitable answers to the questions of the time with our technical expertise. The basis of Phoenix Contact’s decades of growth into a technology leader on the world market is our ability to pick up on technological trends innovatively and quickly”, explained Ronald Bent.

New decade target

The All Electric Society describes a future in which clean electricity is available everywhere at ever lower prices and becomes the core of the energy supply. Through an energy system that is cross-sectoral and based on electricity generated from renewable sources. The All Electric Society’s vision is based on a CO2-neutral future and the implementation of this vision relies on the intelligent coupling of all sectors participating in the energy cycle. Electrification, digitalization, and automation are the keys to this coupling.

https://www.youtube.com/watch?v=YEB_hpByXYI

Digital transformation and the All Electric Society

Via an approach knows as sector coupling, energy will not only be usable in the form of electricity but will also be used in existing infrastructures and technologies like gas pipelines, gas storage facilities, combined heat and power generation, and filling stations. Through the Power-to-X technology, the basis of the energy mix of the future will be hydrogen. To create smart sectors, comprehensive electrification, digitalization, and automation of all areas is needed. Solutions have to be economical and cost efficient though means of energy efficiency and by optimizing the energy and data-related couplings and balancing all energy consumers, generators and potential storage options in the best way possible.

The future concerns us all

In order to create energy efficiency in the consumption and generation of carbon-neutral energy, we must network all sectors participating in the energy cycle, so that they can communicate with each other. Digitalization plays a decisive role here, because without the generation and processing of digital data, this intelligent networking, the so-called sector coupling, will not be possible. This is why we refer to the digital transformation as one of the enablers that makes the All Electric Society possible. 

Join us in introducing new ideas of how we can together bring our successful economic operations into a new dimension.

For more information, please visit www.phoenixcontact.com/all-electric-society

Technology Days: international digital conference on Single Pair Ethernet

From |
Technology days

On September 22 and 23, the SPE System Alliance hosts an international, digital exchange of knowledge between experts of different industries and technology sectors on the topic of Single Pair Ethernet. The Technology Days, taking place for the first time this year, provide participants with the opportunity to talk to specialists and to inform themselves about the added value of this communication technology. A keynote, discussions, and an exhibition constitute the framework of this digital conference. Partners of the SPE System Alliance, like Dätwyler, Fluke Networks, Kyland, Microchip, Phoenix Contact, Prysmian Group, R&M, Rosenberger, Sick, Telegärtner and Weidmüller, will point out trends within SPE technology and explain the relevance for components like switches, semiconductors, sensors, connectors, and cables.

The program will take place at different times on both days so that everyone around the world who is interested in the Technology Days can visit them virtually. The conference will be held in English. If you want to register for the digital conference on September 22 and 23, 2020, please follow this link www.singlepairethernet.com/TechnologyDays. The program can be found here as well. The exhibition will be open for all participants until October 2, 2020.

About the SPE System Alliance The SPE System Alliance is an association of leading technology companies from different industries and fields of application who bundle and exchange their expertise regarding Single Pair Ethernet. All partners thus pursue the common goal of promoting the SPE technology for the IIoT and every other field of application. For more information on the SPE System Alliance, visit www.singlepairethernet.com

Phoenix Contact, Quectel and Ericsson jointly develop the first industrial 5G router for private networks

From |

Phoenix Contact, Quectel and Ericsson have worked together to develop and deploy the first industrial 5G router for local industrial applications in a private 5G network.

With the help of the newly developed 5G Router, industrial applications, such as machines, controls and other equipment, can now be connected to a private 5G network and thus be orchestrated in their resource usage, priority and behavior. They therefore offer a decisive advantage compared to previous mobile radio solutions, which can only use all – mostly license-free – radio bands with a best effort principle and which have to accept performance losses in equal measure when the radio spectrum is heavily occupied.

5G Handshake

To achieve this, all three companies brought their strengths together: Phoenix Contact as the first choice supplier of WLAN, Bluetooth and mobile radio routers for industrial applications, Quectel as the leading global supplier of cellular and GNSS modules and Ericsson supporting the product development as a network supplier and a leading force of the 5G technology development. By starting to interact at an early stage, the three companies have been able to rapidly develop a solution that provides industrial-grade performance over private 5G networks. The collaboration between Quectel, Phoenix Contact and Ericsson has seen extensive interoperability testing at the Ericsson lab to ensure the reliable commercial performance of the 5G router. The experience made is highly important for Ericsson following the strategic approach offering 5G solutions jointly with mobile network operators towards the industry. In addition, all three companies cooperated closely to enable Industry 4.0 applications with this 5G standalone private network. 

To learn more about the different Industrial Communication Standards, please visit the website.

Unmanaged Ethernet Switches Reinvented

From |

Unmanaged Switches from Phoenix Contact enable easy Industrial Ethernet communication. The industrial-grade IP20 and IP67 switches feature variable numbers of ports, various designs, and additional functions such as Power over Ethernet (PoE).

Unmanaged Switches
SFNB unmanaged switches

The SFNB series Unmanaged Switches represent the entry-level solution in our portfolio of Ethernet switches. These switches are particularly suitable for very simple automation applications where there are no exacting demands on the temperature range, data throughput or functions.

Phoenix Contact’s new generation of unmanaged ethernet switches from FL Switch 1000 series offer a narrower housing, greater port density, and best-in-class automation protocol traffic prioritization. The first five variants of the refreshed portfolio are exclusively copper ports, with fiber optic models soon to follow later this year.

unmanaged switches

Both gigabit and fast ethernet models will be included in the initial roll-out, enabling applications of different bandwidths in a variety of industries. With the help of a unique mounting accessory, the FL Switch 1000 series can also be mounted flat on the DIN rail, enabling use in small or flat cabinets with little space. Thanks to Energy Efficient Ethernet, these switches will also feature a reduced power consumption, which will lessen heat and the overall footprint of the device.

More information about the wide range of industrial Ethernet and other products is available on the website.