PHOENIX CONTACT Middle East Employees completed the Great Place to Work® Employee Survey in 2015
The final feedback and results were GREAT! Phoenix Contact Middle East is a Great Place To Work For!

The Great Place to Work survey provides and enables employees, managers and the company as a whole the following:
- Opportunity for feedback and for participation in the cultural development.
- Identifying strengths and opportunities for improvements in the business environment.
- Measurable target tracking in ”Excellence in Leadership” & Communication”.
PHOENIX CONTACT Middle East achieved an 82% Trust Index, thus ranking amongst the Best Companies in the country.
As a result, 94% of employees stated that „Taking everything into account, I would say this is a great place to work.“
About GPTW – Great Place to Work®
GPTW is a global research and management consultancy that recognises the best workplaces in over 50 countries worldwide. Its mission is to improve peoples’ lives and create a better society by improving the workplace experience. GPTW provide a simple, research-driven methodology that could be widely used to understand and assess organisations. Companies from all over the world used this employee survey because they want to create strong workplace cultures based on trusting relationships. In conclusion, Great Place to Work believes that in a society of great workplaces, employees feel respected, proud, and trust. As a result, the management commits to “doing the right thing.”
Read the news on our website.
Our new PSRmini safety relays are rather the narrowest safety relays in the world with the performance of a large safety relay. Phoenix Contact developed the relay technology in the centerpiece of the new PSRmini device. The compact 6 mm wide elementary relay design offers tried-and-tested safety, because of the force-guided contacts. Hence, the numerous technological details make it reliable as safety technology should be. It is its robustness, reliability, and diagnostic capability that sets it apart from a standard elementary relay.
The new DC/DC converters of the QUINT POWER product range are particularly suitable for applications in the energy sector. Independent supply systems can be established and monitored in a preventative manner due to the electrical isolation between the input and output voltage. All DC/DC converters, power supplies, and redundancy modules of the QUINT POWER product range support power boost, which continually supplies 1.25-fold nominal current.