Tag Archives: PROFINET

Power supply for industrial networks

From |

Incorporate Quint DC UPS easily and flexibly into existing networks

DC UPS with IQ Technology for industrial networksContinuing to supply machinery and equipment with power, even in the event of a mains failure, is imperative. Similarly, the ability of the UPS to communicate plays an important role in meeting this requirement. For that reason, we came with the new Quint DC UPS is the first intelligent and network-capable uninterruptible power supply for connecting to the Industrial Ethernet.

First of all, power fluctuations and the failure of the supply voltage generally result in an interruption in operations. In the worst-case scenario, it can result in a total plant failure. Many industry sectors use uninterruptible power supplies, or UPSs for short to avoid this and prevent downtime. This type of solution include three functional units: the power supply, the UPS itself, and the energy storage device. The power supply supplies energy to the load as long as the primary-side mains voltage is present. If the mains fail, the UPS takes over. It switches to the energy storage device so that the connected loads charge with power without interruption. After all, the required power becomes available by the energy storage device. Continue reading

PROFICLOUD – The cloud system for PROFINET

From |

PROFICLOUD is the intelligent solution for the industry

The PROFICLOUD system enables easy and secure communication and control of machines and systems across different locations worldwide. The unique combination of the proven PROFINET standard and Cloud services offers brand new possibilities for automation, including in the Industrie 4.0 environment.

Distributed automation becomes significantly easier with the cloud system, regardless of where your network devices are located. This enables manufacturers to monitor the status of their systems installed anywhere in the world. The evaluation of the data gathered shows, for example, potential failures at an early stage, thereby saving time and money.

Your advanatges

  • You may extend your PROFINET network to include PROFICLOUD services, without requiring any further specialist knowledge
  • Maximum flexibility, thanks to automation across border, from any location, via the internet
  • Easy engineering, as distributed devices and PROFICLOUD network services appear in the local PROFINET network
  • Efficient automation, thanks to preconfigured and preprogrammed PROFICLOUD products
  • Secure communication, thanks to TLS encryption

Furthermore, you can call up data and store it using the cloud services. In addition to current electricity tariffs or the local time, you can also integrate weather data or complex calculations into the PROFINET application.

PHOENIX CONTACT helped shape the trend towards Ethernet-based automation technology from an early stage. Our many years of expertise influence all our products developments, from connectors to programmable logic controllers. By developing our own technology for ASICs, PROFINET controllers or PROFIsafe, we are able to be independent while still ensuring full compatibility with the standard.

Visit our website to learn more about this cloud system technology.