Software-based automation with Virtual PLCnext Control

From |

Greater flexibility and scalability for all system sizes

Virtualization is not new; it was first introduced in mainframe computers in the 1960s. Since 2000, its use has grown and is now widespread in many companies. Phoenix Contact has developed a virtual industrial controller. What advantages does this solution offer for factory automation?

In 2023, the Blomberg-based automation specialist showcased its virtual control activities at the SPS trade fair in Nuremberg. Consequently, this allows IT and OT to collaborate more closely, making automation solutions more flexible and scalable. Furthermore, the Virtual PLCnext Control, based on the established PLCnext Control, extends the PLCnext Technology portfolio. This open ecosystem of Phoenix Contact meets current and future automation needs, combining automation tasks and IoT demands in a single device. Additionally, the ecosystem includes the PLCnext Engineer software platform, the PLCnext Store digital marketplace, the PLCnext Community for sharing expertise, and cloud integration options.

Unlike traditional PLC hardware, the virtual controller is based solely on software (OCI container) and is hardware-independent. This allows installation on industrial PCs and edge devices. Users can create tailored processes without separating the controller from other processes. The virtual controller includes all PLCnext Control functions, supporting industrial protocols and fieldbus systems like PROFINET and Modbus TCP/IP for integrating bus couplers and I/O modules.

Virtual PLCnext

Supplementing the classic PLC hardware

The Virtual PLCnext Control is highly flexible, set up on a Linux server or industrial PC. Parameters like the PROFINET polling rate and connected devices can be freely configured for optimal application. Can it reliably control a crucial production plant? Definitely! Classic PLC hardware also uses industrial PC components, but here, the software is directly installed on the PLC and cannot be significantly modified.

Decoupling hardware in favor of software does not have to entail any disadvantages in terms of automation. Sometimes, the heart of the system is shifted to high-performance servers in an IT cabinet, while hardware, bus couplers, and I/O modules stay in the production system. This is especially useful in large systems or edge applications where data is processed locally. The virtual controller supplements, rather than replaces, classic PLC hardware in an automation portfolio.

Virtual PLCnext

Optimum platform for edge devices

The virtual controller offers more than just replacing conventional PLC hardware and flexible use on large server structures. It benefits edge applications, which involve local data use and evaluation. Previously, this process was separate from automation. Virtualizing control functions removes obstacles between IT and OT. IT can use familiar operating systems to filter and analyze applications or use AI algorithms, generating added value from local data.

On the OT side, the virtual controller, using PLCnext Engineer automation software, is as effective as a classic controller. IT departments can continue operating in their familiar environment without needing new training. Custom license models and quantity structures make the virtual controller suitable for both high-requirement and cost-sensitive projects, avoiding the risk of overdimensioned PLCs for future extensions.

Starter kit based on a compact industrial PC

A hands-on virtual and software-based container may seem contradictory, but Phoenix Contact will present the VL3 UPC Edge at Hannover Messe 2025 as a starter kit for virtual controllers. This compact industrial PC combines the advantages into an edge device. It comes with a user-friendly Linux desktop OS, a container runtime, and preinstalled Virtual PLCnext Control for immediate automation solutions.

Data is collected in the familiar IEC 61131 environment, with the usual Linux environment and PLCnext apps available for evaluation. The high-performance quad-core Intel Atom CPU and 16 GB RAM allow complex analysis to be carried out locally. While not hardware-independent like a PLCnext container, the easy startup of a Linux desktop version enhances the virtual controller’s expandability and user-friendliness compared to classic, minimalist control systems.

Virtual PLCnext control

Convergence of IT and OT

The virtual controller bridges OT and IT in manufacturing, allowing employees to use familiar engineering and programming approaches. It can be cost-optimized and precisely configured for its intended use, with no changes needed for IT users. The open PLCnext Control system supports additional software or apps, and the hardware-independent controller allows for a user-friendly operating system with simple interface support. This approach benefits edge applications by enabling local data collection and analysis. Virtualizing the controller is future-oriented and effective, especially in large systems, allowing for tailored extensions instead of oversized PLC installations.

Become certified and excel in PLC programming

We are excited to offer a PLCnext Technology course in collaboration with iiPD, a leading institute renowned for its innovative technical and professional development programs in Dubai. The PLCnext Technology course is designed to provide participants with a fundamental understanding of Phoenix Contact’s PLCnext platform and the basics of programming using PLCnext Engineer software. Moreover, this comprehensive 3-day course will introduce participants to essential concepts and skills needed to create simple control applications with PLCnext controllers. Enroll now

Learn more about The new Virtual PLCnext Control

Share

Share

Tell your friends

Contact

Leave a Reply

Your email address will not be published. Required fields are marked *