Digital Factory with MORYX

From |

MORYX is a software platform that enables the digital transformation of manufacturing processes. It connects different systems and devices, creates digital twins, and provides flexible and intelligent control options. MORYX is used in 45 applications worldwide. In the following use cases, we want to show which tasks MORYX takes over in practice and which advantages result.

USE CASE: SYSTEM PROTECTION TECHNOLOGIES FACTORY

USE CASE Moryx. SYSTEM PROTECTION TECHNOLOGIES FACTORY. Digital integration of ERP, MES, and PLM.

The “System Protection Technologies Factory,” operated by Phoenix Contact, utilizes MORYX since 2017 for the digital integration of ERP, MES, and PLM systems. MORYX serves as a higher-level digital instance, enabling seamless operation of all systems. The integration has resulted in significant improvements, including zero makeready time for one product line and reduced setup time from 10 to 5 minutes for other lines. The advantages and successes of MORYX’s implementation include parallel production of orders, automated machine setup, handling high product variance, flexible process definition, and accelerated production due to MORYX’s adaptability to changing production environments.

USE CASE: DEVICE CONNECTORS FACTORY

USE CASE Moryx. USE CASE: DEVICE CONNECTORS FACTORY. Digital twin for product, process and machine


Phoenix Contact’s Device Connectors Factory uses MORYX since 2020 to generate digital twins for product, process, and machine, resulting in increased flexibility, control options, and lower scrap.

The advantages of using MORYX’s digital twins include; 10% reduction in production time with optimized first-pass yield, changeover times under 1 minute through parallel production and automatic article management, and the ability to configure production without the need for extensive PLC knowledge. The implementation of digital twins has led to improved production efficiency, reduced scrap rates, and simplified production processes.

USE CASE: MACHINE INTERACTIONS APPLICATION

USE CASE Moryx. MACHINE INTERACTIONS APPLICATION. Smartwatch to notify a skilled worker

Phoenix Contact utilizes machine interaction applications, such as smartwatches to enable seamless communication between machines and skilled workers in one of their plants since 2019. MORYX records real-time machine conditions and messages, sending support requests to plant personnel via smartwatches if problems are detected. The smartwatches provide location-specific details, issue types, severity, and potential solutions, allowing one employee to supervise multiple machines, even across different production halls. The advantages of this system include optimal time utilization, stress reduction for employees, and access to real-time information for efficient decision-making and support.

We accompany you on the way to the Digital Factory

MORYX is a powerful and versatile software platform that can help you achieve your digital factory goals. Whether you want to integrate different systems, create digital twins, or develop interactive applications, MORYX can provide you with the right solution. Feel free to contact us if you have any further questions.

Find out more about Digital Factory with MORYX Here.

Share

Share

Tell your friends

Contact

Leave a Reply

Your email address will not be published. Required fields are marked *