Category Archives: Uncategorized

PLCnext Technology and Virtual PLCnext Control

From |

Combining the tried and tested with the new to create a future-viable solution

The demand for flexible, containerizable control solutions is rising across manufacturing, machine building, and edge computing. Virtual PLCnext Control meets this need as a future‑ready software solution that delivers control functions independently of hardware. It enables classic PLC tasks to run flexibly on powerful server and edge devices while ensuring real‑time performance, scalability, and support for modern languages such as C++, C#, and Python.

Continue reading

High system availability with Power Reliability

From |

Reliable power supply for industrial applications

At Phoenix Contact, “Power Reliability” refers to a comprehensive approach to ensuring system availability in industrial applications. It involves not only supplying electrical energy but also the intelligent interaction of power supply, protection, monitoring, and communication. The goal is to achieve full transparency of the energy system, detect faults early, and proactively prevent failures.

Continue reading

Connection: standard. Design: excellent

From |

The first M17 connector standardized in accordance with IEC

As machines become increasingly compact, every millimeter counts and supply security is crucial. Standardized M17 hybrid connectors provide a smart solution by transmitting signals, data, and power through a single connector, saving space, reducing installation time, and minimizing downtime risk.

Continue reading

Phoenix Contact Trading LLC to Showcase Smart Manufacturing Innovations at Industrial Transformation Saudi Arabia 2025

From |

Phoenix Contact is proud to announce its participation in the upcoming Industrial Transformation Exhibition, powered by Hannover Messe, taking place in just 10 days at the Riyadh International Convention & Exhibition Center. This premier event brings together global leaders in industrial automation, electrification, and digitalization to shape the future of smart manufacturing.

Continue reading

High-availability Ethernet-APL with surge protection

From |

The necessity of surge protection in process engineering systems

Surge protection and equipotential bonding are established in the process industry. In explosive areas, consistent bonding and, if needed, surge protection are essential. The APL products can be integrated into existing grounding and shielding concepts, where high-quality bonding ensures system availability. They allow cable shielding decoupling alongside classic one- or two-sided grounding. For field use requiring maximum failsafe performance possible, the trunk is implemented via fiber optics with an integrated SFP module, though RJ45 remains an option.

Continue reading

Individual configuration, precise and efficient identification

From |

A digital solution for customer-specific marking solutions

Application-specific, standard-compliant identification is key to quality, safety, and availability in industrial plants. Yet evolving requirements, complex standards, and cost pressures pose challenges. Phoenix Contact shows how digital, customer-specific marking solutions support future-proof production.

Using the Marking Configurator, over 2,000 marking materials can be custom-marked and ordered ready to use for industrial identification.
Continue reading