Author Archives: Rehab Saleh

Securely connected with ease

From |

How connector coding increases safety

The star fits in the star, the circle in the circle. This motor skills exercise teaches that only matching shapes connect. Similarly, mechanically coded connectors prevent mismatches, protecting both devices and users.

Whether plugging in a toaster at home, a USB-C phone charger, or an industrial PC, each system uses specific connector patterns to protect users. These patterns prevent incompatible connections, especially for power, signals, and data. While mismatched signal or data lines may fail to work, mixing them with power can damage devices and pose a danger to the user.

Continue reading

Connection technology for heat pumps

From |

Challenges and optimization potential for the installer interface

Heat pumps are vital for the energy transition and reducing carbon emissions. A well-designed installer interface between the pump and building services is crucial standardized connections reduce errors and boost system efficiency and reliability.

Connection technology for heat pumps
Continue reading

Battery energy storage systems as an aid to maximum efficiency and stability in DC power grids

From |

Direct current is gaining importance in industrial and building applications due to its greater stability and efficiency compared to traditional AC grids. Battery energy storage systems (BESS) enhance these benefits in DC grids. Phoenix Contact (Blomberg) and Voltfang (Aachen) have successfully implemented such systems in practice.

Battery storage system in the DC grid of the Phoenix Contact All Electric Society Factory
Continue reading