Monthly Archives: August 2024

Easy mobile marking

From |

Direct, on-site mobile marking for electrical installations

The increasing importance of clear marking in networked components, particularly in plant, control cabinet, and distributor construction, has made the development of mobile printing systems necessary in the field of electrical installation.

On-site marking demands are increasing, necessitating clear and consistent marking of terminals, wires, cables, equipment, and systems, as well as compliance with a growing list of standards.

Digitalization of marking processes

Phoenix Contact introduces the THERMOMARK GO thermal transfer printer. A mobile system solution that offers high flexibility, short working paths, and no accidental double processing of missing markings. The printer, software, and marking materials – THERMOMARK GO – are all integrated with the MARKING system app, allowing easy smartphone interaction with the printer.

Continue reading

Storing energy in an All Electric Society

From |

Climate change and population growth are posing a global challenge. How to stop global warming and increase energy consumption while protecting the climate? The All Electric Society vision aims for a sustainable, affordable energy system where renewable sources, such as sun, wind, and water, are used. Researchers at Oregon State University predict that photovoltaics could cover all energy requirements globally, using less than 1% of the earth’s surface. However, achieving this energy revolution requires extensive renewable energy expansion of renewable energy and the technological approach of sector coupling.

Battery storage systems

Sector coupling

Sector coupling involves the comprehensive electrification, networking, and automation of all relevant areas of our lives and economies. Including industry, energy, mobility, infrastructure, and buildings. In the All Electric Society, these sectors are networked to create a self-controlling system that optimizes energy efficiency and energy savings by balancing loads, producers, and storage systems. This ensures stability and availability of power supply without excess capacity. Making energy storage systems a core element of sector coupling.

The role of energy storage systems in an All Electric Society

To ensure a stable power supply based on renewable sources like sun, wind, and water, reliable storage systems are necessary. There are various technologies for temporarily storing electrical energy, with the main difference being their physical principles. Mechanical storage converts electrical energy into mechanical energy. While purely electrical storage uses capacitors or inductors. Electrochemical storage uses electrochemical potentials and electrolytes to store electrical energy in batteries. Thermal storage generates heat and drives electrical generators.

The role of energy storage systems in an All Electric Society
Continue reading

Fiber optics

From |

High-speed data transmission for industrial applications

IDC predicts that by 2027, the volume of data created and replicated will reach 284 zettabytes, a 21-zero figure, threatening the Internet of Things without a nationwide broadband expansion, highlighting the need for significant data storage and replication.

The first transatlantic fiber-optic cable was operational in 1988, enabling high-speed data transmission between continents. The mid-1990s saw broadband expansion, adding more long-distance routes and moving fiberglass transmission paths closer to end devices like data centers, industrial plants, and personal computers, known as the “last mile.”

Data transmission across continents, countries, and municipalities requires high security and reliability. Speed, immunity to interference, and failsafe performance are basic requirements for industrial and semi-industrial data transmission.

The advantage of fiber optics

Fiber-optic cables (FO) transmit data in light over long distances by converting electrical signals into photon packets and sending them to the receiver via plastic or fiberglass. The light signals are then converted back into electrical signals for evaluation and processing.

This blog article explores the advantages of data transmission through fiber-optic cables over copper transmission, focusing on their characteristics.

Speed and distances

Fiber-optic cables use photons to transmit electrical signals, which are faster than electrons in copper conductors. Photons can travel up to 70% of the speed of light, with minimal signal loss. This allows for longer transmission distances of up to 50 km and data rates of up to 40 Gbps. The actual range depends on the chosen fiber-optic cable, making them suitable for long distances and large data volumes.

Reliability and security

Fiber-optic cables are reliable for data transmission due to their non-conductive cores made of glass or plastic, eliminating the need for complex shielding. They are metal-free, insensitive to EMC and ESD interference, allowing parallel use with other cables. Impedance problems and crosstalk are not issues. Fiber-optic cables with coatings protect against environmental influences in a much better way.

Fiber-optic cables offer enhanced cybersecurity due to their lack of external signals, requiring direct access via bend connectors or contact points, making them significantly more secure against eavesdropping than copper cables, despite not providing 100% protection against unauthorized access.

Costs

Fiber-optic technology has disadvantages such as complex assembly, precision, expensive equipment, complex measurement technology, and the need for well-trained specialists. Manufacturing and monitoring production are costly and require extensive expertise in this specialist field.

Continue reading

Functional safety for analog signals

From |

Simple implementation with the PSRmodular and AXL F series

Phoenix Contact offers two series of analog signals for monitoring physical variables in process engineering systems. These signals are standardized as either a (0)/4 … 20 mA or a 0 … 10 V signal, with current signals being more robust against electromagnetic interference and having high measuring accuracy over longer cable lengths. Furthermore, the concept considers whether the sensor is powered by the evaluation module or supplied by an external source.

Functional safety for analog signals

Consideration of load and measurement information

The analog evaluation module distinguishes between active and passive inputs, requiring external supply for passive inputs. Load consideration is crucial when engineering analog signals, and signal conditioners are recommended if it exceeds active inputs. Moreover, NAMUR recommendation NE43 defines signal levels for failure information of digital measuring transducers with analog output signals, with current values outside these limits considered invalid or failure information. The evaluation unit must provide corresponding information or respond to deviations.

Design of functional safety

Single-channel analog signal generators can be used for safety-related circuits up to SIL 2/PL d. While two-channel signal generators can be used up to SIL 3/PL e. MTTFD values can be determined based on sensor manufacturer failure rates. Furthermore, Diagnostic coverage (DC) is required for safety-related analog signals, but plausibility comparison is difficult due to measurement inaccuracies and ambient conditions. Two-channel architectures should allow short-term deviations outside the tolerance range, without impacting functional safety.

Continue reading