Modernizing and digitalizing process plants
The process industry is in a state of change
In many production operations, control systems from different manufacturers and different generations are in use due to long runtimes – many systems are already decades old. This results in a corresponding pressure to modernize process systems. The way to a modern, digital plant is based on a three-step plan. The goal is to bring the communications up to the state of the art so as to optimize maintenance processes, reduce unplanned failures, and make inspection rounds paperless.
Never change a running system – this phrase fits especially well to the process industry. Many chemical plants are often more than 20 years old and need to be modernized because built-in devices were discontinued or more efficient components became available. Process plant operators are retrofitting in order to gain more reliability and reduced downtime. With Phoenix Contact, valuable space in the switch cabinet is optimized and applications are made ready for future requirements.