Tag Archives: automation

PLCNext – Limitless Possibilities

From |

Written by Andrew Ellis – Field Application Engineer, Automation and Renewables

As an automation engineer with nearly 20+ years of experience with multiple automation systems across many industries,  you would think that answering questions on automation products would be easy. However, having recently joined Phoenix Contact, one of the more difficult questions I get asked is how would I describe PLCnext?

My first thought is to equate PLCnext to a blank piece of paper. With a pencil you can draw and create plans. Scissors allow you to cut out shapes, and folding the paper with your hands allows you to build. Tools are what make PLCnext so flexible. With the ability to program in IEC 61131, C++, Matlab, Python, Rust, Node Red etc you can find the right tool for the job. PLCnext provides the flexibility of Linux, with the reliability of a PLC.

Then I think to myself, maybe a better analogy would be with a multitool. PLCnext provides a single platform for small scale systems, through to full scale decentralised systems and also edge computing. Extension modules provide further functionality with PROFIsafe, IO link, Machine learning and of course, compatibility with the full range of Axioline IO modules and remote IO.

Or maybe it should be likened to a mobile phone. The PLCnext store allows you to extend the functionality of the system with pre-built software extension, or you can download fully realised apps directly to your controller. Furthermore, if you have an app you wish to commercialise, then let us assist you to take advantage of our eco-system and sell your app on the PLCnext store. Phoenix Contact also provide a social space to exchange ideas and support each other within the PLCnext community.

For more information about PLCnext, contact Andrew on 07584514958 or email aellis@phoenixcontact.com

Or maybe I just need to ask what ideas do you have for your next product? Then we can demonstrate how PLCnext can be open to your automation possibilities, rather than limit your solution.

Introducing Axioline Smart Elements

From |

Written by Tony Deane, Technical Manager

These days everyone wants more for less and as we all know, if the market demands something you must respond accordingly to stay ahead of the curve. Phoenix Contact have listened to the marketplace and launched an innovative, revolutionary and competitive I/O system to complement and enhance our AXIOLINE I/O range for the automation industry!

Introducing the AXIOLINE Smart Elements I/O range

With panel space, easy start-up and component costs being some of the major requirements of systems builders, the marketplace demands suppliers to react in order to help businesses maximise production and profits and minimise costs. Together with the system fieldbus options offered by the Axioline I/O system, Smart Elements is a definite game changer.

Continue reading

The Axioline P Process I/O Platform

From |

Written by Tony Deane, Technical Manager

“One small step for Phoenix Contact. One giant leap for the Process Automation industry”

In today’s current climate of digitalisation and IIoT, there is a major trend going on across all industries. Namely users are demanding more information from their plant with the goal of optimising assets to improve operating performance.

The increased demand is pushing Ethernet to move further out into the plant, closer to field devices. However, in terms of integrating Ethernet into process instrumentation at the device level, we are some way from that point.

Continue reading

Good things come in small packages

From |

Written by Tony Deane, Technical Manager

This has never been more apt than when it comes to our new I/O system Smart Elements.

Today, more and more within the machine building industry, the push for system enclosure sizes to be kept to a minimum demands a compact footprint within the control cabinet. There is also the ever present drive to save time and money on builds. Axioline Smart Elementsrises to these challenges and delivers spectacularly!

Continue reading

Compact industrial PCs

From |

Written by Gareth Chamberlain, Product Manager- Cyber Security & IT Automation

An industrial PC is normally the last thing on many developers’ / integrators’ minds when designing an application. The process of selecting an IPC can also be a daunting task when selecting the specifications- this is where our knowledge of industrial computing can help you to decide the correct unit for you.

With more decentralised systems becoming more prominent within the automation community and EDGE/FOG computing, Phoenix Contact launched a new range of IPCs at the SPS show in Nuremburg in November. Our new range of IPCs are designed with high performance for its class and the usual Phoenix Contact rugged quality.

Introducing the BL2 BPC 1500:

  • Metal compact housing
  • Intel Celeron N3350 processor
  • Microsoft Windows 10 and Linux are supported
  • M.2 Storage options
  • Serial Port (optional)
  • WLAN 802.11 (optional)

With the size of the housing 97 x 95 x 49 mm (without the optional COM ports) there are a huge array of applications this can run within.

The BL BPC 1500 industrial PCs will be available from 1st of January 2020.

Phoenix Contact has a wide portfolio of industrial PCs that can help you in your application. If you have any questions regarding the BL BPC 1500 or need help in your selection of an IPC that will fit your project please contact us.

For more information, contact Gareth on 07946 757375 or email gchamberlain@phoenixcontact.com

Automation made easy…?

From |

Written by Andy Maskell, Product Manager- Safety, I/O & Networks

Automation continues to develop at a very fast pace but the complexity can also increase and in turn the skills required to make it work. There is no sign this trend is slowing down but what we still see is the need for cost effective and easy to implement solutions that remove the need for software licences, complex programming and expensive hardware for smaller applications that still need to be automated.

Continue reading

The Future is Electric

From |

Written by Duncan Nicol

For thousands of years we have relied on carbon fuels to power our world and for a long time, it made a lot of sense. Carbon fuels such as coal and oil were easy to get to and therefore a cheap source of fuel and energy dense. As demand increased they became harder to find and then, of course, the environmental impact became widely known, but by then we were so very dependent on them. Continue reading

Discover the latest in energy and transport technology at Fully Charged Live 2018…

From |

Written by Nigel Dawbarn

In a couple of weekend’s time, we will exhibit at “Fully Charged Live” at the Silverstone Circuit. An exhibition of energy and transportation technologies, with an, Ask the Expert area and lots of theatre sessions including panel discussions around the subject of Electric Vehicles in the UK. Hosts include Robert Llewellyn, Jonny Smith and Helen Czerski from the YouTube show “Fully Charged”

car_charge_image

Continue reading