Tag Archives: Power supplies

The QUINT power supply is 25 years old

From |

Happy Birthday to you, happy birthday to you, happy birthday dear QUIIII-INT, happy birthday to you! 

This year marks 25 years since the first QUINT power supply was released. That’s back in 1996 when just 5 power supplies were released to the market. Fast forward to today and there are more than 100 QUINT products available with the QUINT4 being the most recent iteration.  

So how have we seen the QUINT develop over this time?  

Obviously, they have become smaller and more efficient, for example our second-gen QUINT 40A (only just discontinued) was the size of a small breeze block at a width of 240mm. Compare this to the QUINT4 version which is exactly half the width at 120mm.  

The QUINT now packs many more technical features and benefits that make it the #1 choice for markets and applications where reliability and power resilience is key.  

Some features that have been added and are now the norm are such things as: 

  • Boost Power, both dynamic (short term) or static (permanent)  
  • SFB – selective fuse breaking, a high current boost enabling fast tripping of breakers or even fuses.  
  • Better monitoring & diagnostics with configurable digital outputs and an analogue output 
  • High reliability and long lifetime, typically 15 years. 

QUINT is not just a power supply range (available from 1A to 40 A), the range includes DC/DC converters, redundancy modules, uninterruptible power supplies and energy storage devices including various battery technologies, buffer and Cap modules.   

The complete QUINT solution for maximum plant availability can be seen via the following link. Here you will find info on all the products under the QUINT banner including a live demo showing our intelligent communicative QUINT4 UPS.  

The near future will see more development in the area of communication, including IO Link and easier integration with complementary Phoenix Contact systems such as electronic circuit breakers. I would not be surprised if a fifth generation QUINT is not already under development.  

The QUINT power system is part of the COMPLETE line system. 

For more info contact Mark on 07717 335477 or email  mlloyd@phoenixcontact.com 

Capacitor based storage systems – an alternative to batteries?

From |

Written by Mark Lloyd, Senior Product Manager- Power Supplies & Surge Protection

I have been involved with UPS systems for more years than I care to think of, and I can say that if a customer ever has a problem with a UPS more often than not it is the battery that is the issue.

At the end of the day a battery is essentially a box full of chemicals and they have to be treated with a certain amount of care. If a battery is left on a shelf in storage for too long without first being charged, the battery will self-discharge. It depends on the size of the battery (AH) but, typically, the larger the battery capacity, the longer the time you have before the battery needs to be recharged. Once it is charged you have a similar amount of time before it needs to be charged again if it is not put to use right away.

Continue reading →

Feel the power

From |

Written my Mark Lloyd, Senior Product Manager- Power Supplies & Surge Protection

The 1st Standard DIN RAIL power supply with 110 VDC output.

Up until now, the highest output we could achieve with one PSU was 56VDC using a 48DC power supply turned up to its maximum voltage. In order to achieve the higher voltages for which we are regularly asked, it was only possible with two wired in series. For example two series connected 48DC nominal power supplies individually “tweaked” up to 55DC.   

Continue reading →

Protect your most sensitive equipment

From |

Written by Mark Lloyd, Senior Product Manager- Power Supplies & Surge Protection

If you were to ask any electrician or plant maintenance engineer what the main reasons are for electrical equipment failure, some of the answers would be insulation degradation, poor grounding, bad connections but I would put money on voltage spikes as being one of the top answers…..

Voltage spikes can be harmful to electrical and electronic devices and increasing the voltage above a devices nominal operating voltage can cause internal arcing and heat generation that can cause damage to circuits, and with devices becoming smaller and more sophisticated this increases the likelihood of this kind of damage. Often if damage occurs within the devices usually warranty period, the cause may not even be identified. 

Continue reading →

Maximum power, maximum safety

From |

Written by Mark Lloyd, Senior Product Manager- Power Supplies and Surge Protection

For critical applications within the process industry (and increasingly from other sectors) it has long been common practice to use redundant power supply systems. Previously this has required 2 or more separate power supplies decoupled from each other using either diodes or for more sophisticated systems, redundancy modules.

Continue reading →

Combined power supply and UPS – just add battery…

From |

Written by Mark Lloyd, Product Manager- Power Supplies & Surge Protection

For nearly 10 years, the TRIO combined power supply/UPS has been on the market and has become one of our most popular UPS. This year, it has been given a makeover with the release of the 2nd generation TRIO DC UPS.

Trio UPS

Paraphrasing something I have heard on numerous occasions from customers: “We really like the concept of a combined mains input power supply and 24DC output UPS, but at only 5A we really could do with more power”.

Continue reading →

Is your power supply ready for the Industrial Internet of Things? The QUINT4 DC UPS sure is.

From |

Written by Mark Lloyd

monday_blog_img1

In 2004, we released our first DC UPS, the first generation QUINT-UPS, which is still in use and purchased today.

Then in 2011, we released the QUINT UPS-IQ, which for the first time allowed some monitoring of the connected battery to see such things as battery status, battery lifetime, and remaining runtime. With this generation of UPS it is possible to pass this info up to higher level controls but requires additional hardware.

Continue reading →

Expanding range of UPS for AC applications

From |

Written by Mark Lloyd, Product Manager- Power Supplies & Surge Protection

For many years the use of Uninterruptible Power Supplies or UPS in the control cabinet have been the domain of the DC UPS, by which I mean mains in and low voltage DC out. Less common is the use of AC UPS, by which I mean mains in and mains out.

QUINT AC UPS In certain sectors, such as Water/Wastewater it has been common practice for some years to use what I would call commercial grade AC UPS, such as you would find in office IT applications.  Because these UPS are not designed for industrial applications they are usually just sat in the bottom of the cabinet. Not a very elegant solution.

Continue reading →