Written by Fraser Cowie, Product Manager- Interface
It only seems like yesterday that we launched the 1st iteration of the innovative and unique Contactron Hybrid Motor Starter, but in fact this year sees its 13th birthday.
The Contactron offer has evolved several times since that starter was released – see if you can remember all the different variants that have been produced since that momentous day:
2008 – the very first 4 in 1 hybrid motor starter is launched. This revolutionary 22.5mm wide fixed speed motor starter has forward and reverse, motor protection and emergency stop functionality.
Continue reading


What you may have noticed recently is the change of colour. The original green (RAL 9010) is replaced by a smarter more ergonomic grey (RAL 7035) – the size and functionality of the starters remain