Tag Archives: circuit breaker

Turn your circuit breaker into an IoT enabled device

From |

There are number of trends in the world of automation, one of the more recent ones is the increasing use of circuit breakers designed specifically to protect DC lines. So called electronic device circuit breakers are fast replacing standard AC circuit breakers as the first choice.  Despite AC breakers being lower cost the technical advantages of DC electronic breakers to protect critical loads and the peace of mind that brings is driving a rapid growth in their usage.

One of our more popular products is the 4 channel CBMC electronic circuit breaker. Each channel can be individually set up to a maximum of 10A to protect the connected loads. In our Vlog we are featuring a version with an IO-link interface which now enables remote access to the device via platforms such as Proficloud.

Continue reading