Written by Fraser Cowie, Product Marketing Manager- Interface
Customers today want smaller, more energy efficient products that won’t cost a fortune to run and will fit into smaller and smaller control cabinets.
With these issues in mind Phoenix has just released their latest switch mode DC power supply called UNO.
Here are 10 reasons why to choose UNO:
- The range is over 90% efficient
- It has extremely low losses in the no load condition of less than 0.3 watts
- The offer has a 10 to 20% higher power density than its nearest competitor, giving it the highest power density in its class
- It has a MTBF of greater than 500,000 hours
- It incorporates the latest generation of ASIC (application-specific integrated circuit) circuitry, more powerful and more energy efficient than previous models
- The range is made from high impact resistant plastic that means a better EMC behaviour and reduces costs as there is no need to provide an earth wire
- It has an extended ‘hiccup’ mode which means it can be used to start low power motors or capacitors of greater than 20.000 µF
- It has a wide temperature range of -25°C…+70°C
- It has Worldwide approvals including UL
- It comes in 12volt and 24 volt output versions up to 100W
All these features make a great argument to start using the UNO power supply offer, so go green today!
UNO is not the only power supply offer from Phoenix Contact.
QUINT POWER: power supply units for maximum system availability
TRIO POWER: power supply units with basic functionality at the highest level
MINI POWER: power supply units for measurement and control technology
STEP POWER: power supply units for installation distributors