Written by Gareth Chamberlain- Technical Support Engineer (Automation)
Quick question? Do you know who is looking at your data on-site or remotely?
With the recent events in the Ukraine can you afford to take that risk? The December 23rd outage at the Prykarpattaoblenergo Power plant in the western region of Ukraine suffered a scenario that few organisations would want to experience.
The power outage was caused by a compromised computer, with a small executable application within the system. This malware targets SCADA systems and infects, silently searching for systems that it can control. The name of this Malware is “Blackenergy” – a small piece of code that can bring down systems and has brought misery to over 80,000 people.
At Phoenix Contact, we are very aware of these threats and we have created a solution that would isolate a SCADA system from attacks. The mGuard, a network firewall, creates a barrier between your production equipment and your corporate network.
“Why do I need another firewall ? Doesn’t our IT department look after that?”
In the world of Cyber Security it only takes one system to be compromised to be a real threat to the entire network. Once the malware has passed through the firewall there is a 70% chance of the code infiltrating the system if Antivirus software is installed- 100% if no antivirus is installed.
The mGuard creates an island that can be separate from the rest of the network, giving you peace of mind. The mGuard uses state of the art, military grade encryption to keep you and your data safe. This application also allows VPN, remote monitoring to trusted people only. You control who enters your network and who does not. With mGuard, you are in control.
For more information on mGuard security products please contact Andy Maskell tel: 07584 235440 or email amaskell@phoenixcontact.com.