10 Reasons to Go Green with Phoenix Contact!

From |

Written by Fraser Cowie, Product Marketing Manager- Interface

Customers today want smaller, more energy efficient products that won’t cost a fortune to run and will fit into smaller and smaller control cabinets.

With these issues in mind Phoenix has just released their latest switch mode DC power supply called UNO.

 Uno1

 Here are 10 reasons why to choose UNO:

  1. The range is over 90% efficient
  2. It has extremely low losses in the no load condition of less than 0.3 watts
  3. The offer has a 10 to 20% higher power density than its nearest  competitor, giving it the highest power density in its class
  4. It has a MTBF of greater than 500,000 hours
  5. It incorporates the latest generation of ASIC (application-specific integrated circuit) circuitry, more powerful and more energy efficient than previous models
  6. The range is made from high impact resistant plastic that means a better EMC behaviour and reduces costs as there is no need to provide an earth wire
  7. It has an extended ‘hiccup’ mode which means it can be used to start low power motors or capacitors of greater than 20.000 µF
  8. It has a wide temperature range of  -25°C…+70°C
  9. It has Worldwide approvals including UL
  10.  It comes in 12volt and 24 volt output versions up to 100W

Uno2 Uno3

All these features make a great argument to start using the UNO power supply offer, so go green today!

UNO is not the only power supply offer from Phoenix Contact.


QUINT POWER
:      power supply units for maximum system availability

TRIO POWER:         power supply units with basic functionality at the highest level

MINI POWER:         power supply units for measurement and control technology

STEP POWER:          power supply units for installation distributors

 

Uno5

More information about Phoenix Contact’s Power Supplies

Share

Share

Tell your friends about us!

Contact

Leave a Reply

Your email address will not be published. Required fields are marked *

Time limit is exhausted. Please reload CAPTCHA.