Written by Duncan Nicol, Market Segment Manager- Device Connections.
Product design is all about form and function, both of which are well understood at Phoenix Contact as innovators of smart device connection technology. The connector is an integral part of any device and, if carefully selected, can enhance and improve the functionality and usability of the device.
Within industry, energy costs are continually increasing. As a result reducing energy costs is becoming increasingly important in terms of providing companies with a major competitive advantage in the areas of production, process and industrial engineering.
The new PT Power 95 high-current terminals make it possible to connect and wire rigid or flexible ferruled conductors up to 95 mm² directly and without the need for tools.
7.2Mbps.
So here we are once again with my last blog of 2013 so I thought I would highlight not only a very innovative technology but also a very new market. Building-integrated photovoltaics, or BIPV as it’s more commonly known, is the latest trend in energy development using solar technology.