Tag Archives: toolfox

Fancy a bit more time?

From |

Written by Andy Neat, Senior Product Manager – Marking & Identification and Toolfox

Morning and welcome to another Monday morning Blog from myself. I hope you’re all well and that life has started to normalise for you slowly. 

What takes the most amount of your time daily? Assembly? Picking? Wiring? Marking? Testing? Well, if the answer to that is wiring then we can help you out with some time saving tools to help streamline your processes. 

The tools listed below are not only huge time saving pieces of equipment but also on a special offer for the rest of this year. 

The CF 3000 will strip and crimp your wires in less then 2secs… 1.2secs to be precise! The time saved on this machine is approx. 4x over a minute. The CF 3000 will strip and crimp wire sizes of 0.25mm, 0.5mm, 0.75mm, 1mm, 1.5mm and 2.5mm that are supplied on a strip of 50pcs. 

Continue reading