Tag Archives: quint4

Is your power supply ready for the Industrial Internet of Things? The QUINT4 DC UPS sure is.

From |

Written by Mark Lloyd

monday_blog_img1

In 2004, we released our first DC UPS, the first generation QUINT-UPS, which is still in use and purchased today.

Then in 2011, we released the QUINT UPS-IQ, which for the first time allowed some monitoring of the connected battery to see such things as battery status, battery lifetime, and remaining runtime. With this generation of UPS it is possible to pass this info up to higher level controls but requires additional hardware.

Continue reading →