Tag Archives: Interbus

Back To The Future: Interbus Obsolescence

From |

Written by Tony Deane, Sales & Marketing Manager- Industry Management & Automation

Interbus is still an integral legacy part of industry, still supporting and operating countless systems throughout several industries from Automotive, Food and Beverage, Printing, Materials Handling and many more.

One of the defining characteristics of many Interbus systems is that, in many cases, they are spread over a wide area within a factory. In fact, due to the integrated repeater function in each device, the total expansion of the INTERBUS system can reach 13 km (8.078 mi.). Replacing a controller is one thing, replacing an entire network infrastructure of that magnitude on an operationally critical system to a business is an entirely different proposition and undertaking which, if at all possible, you would want to avoid.

The issue facing many legacy Interbus users is that many vendors who, in the past, used Interbus to leverage its ground-breaking properties when launched in 1986 (and used in new installations up to as recently as 2013), no longer support the PLC Systems that used Interbus as a fieldbus network, or no longer supply the Interbus master interface card, as the factory automation industry moves away from serial copper based network technology to Ethernet based networks (Profinet, Ethernet IP, Ethercat).

So, the question is how can you upgrade your control system to the latest control technology without having to replace a perfectly robust, extensive, and functioning network infrastructure overnight?

As the creators of Interbus in 1986, Phoenix Contact offers you not one, but two options.

Firstly, we offer the FL NP PND 4TX 2985974 Profinet proxy device.

The FL NP PND 4TX device allows your control system to control your Interbus network by combining a Profinet device with an integrated Interbus G4 Master within one product.  The device allows the PLC to talk to the Interbus network via Profinet. This will provide a path towards a gradual change of network infrastructure, whilst the plant remains in operation.

For the second option, Phoenix Contact offer PLC Next Technology utilising the AXC F XT IB 2403018 Interbus master interface. This option requires a far more comprehensive re-engineering approach than the FL NP PND 4TX but will allow you to bring an existing, robust and dependable Interbus system into a control platform that can leverage High level languages including C#, C++, Opensource software, allow you to use the likes of NodeRed and allow instant IIOT cloud access to process data via Amazon Web Services, Microsoft Azure and our own Proficloud service to give visibility and transparency, to enable early diagnosis, intervention and ultimately, efficiency to your system.

Both solutions allow for a gradual migration to Profinet over an extended period, therefore making the inevitable move to an Ethernet technology-based network, a project-based undertaking with less disruption both operationally and financially.  

For more information or demonstration of either option contact Tony Deane on 07824 437393 or email tdeane@phoenixcontact.com

Do you have Interbus legacy and obsolescence concerns?

From |

Written by Tony Deane, CST Technical Manager

Since 1987, Interbus has been, and still is, a reliable and robust network that continues to provide solid fieldbus solutions throughout industry across the wide spectrum of the automation landscape from the food industry through to printing and automotive.

Proxy for PROFINET-RTMany companies still rely on this enduring backbone to run their automation processes and shop floor infrastructure. However, with the move towards Industry 4.0 and The Internet of Things, it is accepted that Ethernet based networks are now the only way forward.

But what about the perfectly sound Interbus infrastructure in place already?  Thousands of sites across the world cannot be expected to remove a perfectly functioning network just for the sake of it!

Continue reading

Interbus is alive…

From |

Witten by Gary Trewhitt, Business Development Manager- Automotive

So Interbus is dead. “LONG LIVE THE QUEEN”.

Who said Interbus is dead?

Not an uncommon misconception, as others would have you think.

Perhaps Phoenix Contact took its eye off the ball in relation to Interbus? I would say forward thinking.

Interbus is alive and truly well.

Interbus-Brain

Continue reading